Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release14 April 2023Digital IndustriesNuremberg
First virtual Simatic controller enables more flexible, software-based automation

The first virtual controller from Siemens is based on the functions of an S7-1500 hardware PLC and is made available via Industrial Edge.
Benefits of the virtual PLC for users
And that’s exactly what the
new, virtual controller offers, since users can now also use proven functions
of the S7-1500 hardware controller in the digital world. The virtual PLC is
hardware-independent – in other words, no specific hardware is needed. Industrial
Edge Management makes it possible to manage the virtual controller and other
applications at a central level and adapt them flexibly to customer needs. Individual
services can be booked and used in addition, so costs can be optimized. This
kind of data-centered and software-based automation enables customers to
respond more flexibly. “If the service specialists are
not in the factory at a given moment, they will be sent a diagnostic message to
say the controller has stopped, for example,” says Efrossini Tsouchnika, Vice
President Control at Siemens. “The Industrial Edge Management System gives them
the ability to access the virtual controller remotely. That means they can
get the plant running again with no obstacles to action.”
Thanks to the virtual
controller, PLC projects are easier to scale, and open data interfaces mean
they can be readily integrated into other IT offerings. The Simatic S7-1500V is
fully compatible with the TIA portfolio. Customers can thus re-use projects and
data already in the TIA Portal and reduce their level of investment.
Increasing convergence of IT and OT
Using the Simatic S7-1500V,
Operational Technology (OT)-oriented users can continue to use their trusted
structures while benefiting from the advantages of an IT-oriented environment. But
users accustomed to IT can also work in a familiar environment using the
digital controller. That simplifies the collaboration between automation
engineers from the world of OT and software users in the IT field, and further
advances the fusion of these two environments.
For further information on the Simatic S7-1500V virtual controller:
www.siemens.com/virtual-plc
www.siemens.com/virtual-plc
Further information about Siemens at Hannover Messe 2023 can be
found at: www.siemens.com/presse/hm23 and
www.siemens.com/hannover-messe
For this press release
Follow us on social media
Siemens Digital Industries (DI) is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI’s unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has around 72,000 employees internationally.
Siemens AG (Berlin and Munich) is a technology company focused on industry, infrastructure, transport, and healthcare. From more resource-efficient factories, resilient supply chains, and smarter buildings and grids, to cleaner and more comfortable transportation as well as advanced healthcare, the company creates technology with purpose adding real value for customers. By combining the real and the digital worlds, Siemens empowers its customers to transform their industries and markets, helping them to transform the everyday for billions of people. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a globally leading medical technology provider shaping the future of healthcare. In addition, Siemens holds a minority stake in Siemens Energy, a global leader in the transmission and generation of electrical power.
In fiscal 2022, which ended on September 30, 2022, the Siemens Group generated revenue of €72.0 billion and net income of €4.4 billion. As of September 30, 2022, the company had around 311,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
In fiscal 2022, which ended on September 30, 2022, the Siemens Group generated revenue of €72.0 billion and net income of €4.4 billion. As of September 30, 2022, the company had around 311,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Reference Number: HQDIPR202304136682EN