Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release07 June 2018Process Industries and DrivesNuremberg
First pressure transmitters for remote commissioning of functional safety

The picture shows the pressure transmitter Sitrans P320/420 from Siemens.
The HART7 Sitrans P transmitters are ready for plant digitalization, giving users in-depth control and analysis through new data logging functions and event control. The devices' reduced response time increases process efficiency by speeding up the control system's response to changing process conditions.
Sitrans P320/420's user-friendly features also include a new larger and improved display, showing users the device's status at a glance. Setup is convenient and quick thanks to four-button programming, Namur NE107 support and a quick start wizard.
With measuring ranges from 20 mbar to 700 bar, depending on the device, these new additions to Siemens pressure portfolio provide reliable results even under extreme conditions. The devices are especially suited for applications where safety is critical: in industries such as chemical, oil and gas, and power generation. The Sitrans P320/420 can also be implemented in all other industries.
Further information is available at www.siemens.com/pressure
Find further information about Siemens at the Achema 2018 at www.siemens.com/achema and www.siemens.com/press/achema2018
For this press release

Event: Achema 2018
Press Event
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 377,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
David Petry
Siemens AG
Werner-von-Siemens-Str. 65
91052 Erlangen
Germany
91052 Erlangen
Germany
+49 (9131) 7-26616