Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release10 January 2019Power and GasHouston
Encana selects Siemens to provide rotating equipment for Pipestone Processing Facility

Siemens' SGT-750 turbine offers customers lower life cycle costs compared to competing turbines in the industry.
The first train will consist of a Siemens SGT-750 gas turbine driving two Dresser-Rand DATUM compressors for feed and sales gas compression, combined with a Siemens waste heat recovery unit for process heat. The second train will consist of a Siemens electric motor-driven DATUM compressor for refrigeration compression with Siemens variable frequency drive.
"Siemens state-of-the-art SGT-750 gas turbine is the only twin-shaft engine in its power class with industry-leading fuel efficiency and one of the lowest emission profiles," said Patrice Laporte, Vice President, Oil & Gas for Siemens America. "The train configuration achieved by coupling the SGT-750 with the highly efficient DATUM compressors provides an excellent solution for the Encana's Pipestone gas compression service."
The SGT-750 turbine has a proven track record of satisfied customers in both power generation and mechanical drive applications and is becoming an increasingly popular choice among facility operators. In 2015, Siemens supplied three pipeline compressor trains driven by SGT-750 gas turbines to Central America-based Fermaca for its El Encino – La Laguna pipeline project. In 2017, China's largest acrylic producer, Zhejiang Satellite Energy Co., selected Siemens to provide an SGT-750 gas turbine to drive two Siemens STC-SH single-shaft compressors for Phase II of its propylene dehydration plant.
"We're providing all of the equipment for these two compression trains from one source, which lends testament to Encana's ongoing confidence in our equipment and Siemens' capability to offer a one-stop solution to our customers," said Matthew Chinn, Executive Vice President New Equipment Solutions for Siemens Oil and Gas. "Further to this, our solution is less capital intensive, due to the excellent attributes of the SGT-750 turbine's lower life cycle costs compared to competing turbines in the industry."
With maximized uptime and a low environmental emission footprint, the SGT-750 offers customers a lightweight industrial gas turbine designed and developed to incorporate the size and weight advantages of an aeroderivative gas turbine while maintaining the robustness, flexibility, and longevity of traditional heavy-duty industrial gas turbines.
The DATUM compressor line is known for its efficiency, reliability, and ease of maintenance which makes these compressors ideally suited for the un-spared feed / sales gas and refrigeration compression applications. In 2015, Encana purchased 10 DATUM compression trains for its Cutbank Ridge Program, designed for the long-term development of natural gas resources in Northeast British Columbia.
For further information on the SGT-750 gas turbine, please see https://sie.ag/2ORY764
For further information on the DATUM compressors, please see http://bit.ly/2Ms5zbz
For this press release
@Siemens_Energy
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2018, which ended on September 30, 2018, Siemens generated revenue of €83.0 billion and net income of €6.1 billion. At the end of September 2018, the company had around 379,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Janet Ofano
Siemens AG
5101 Westinghouse Boulevard
28273-9640 Charlotte, NC
USA
28273-9640 Charlotte, NC
USA
+1 (803) 389-6753