Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release02 August 2017Process Industries and DrivesNuremberg
Effective plant asset management – new functionalities for smart field devices
The Simatic Process Device Manager forms the basis for data and status monitoring of smart field devices in the maintenance station. Simatic PDM is a universal, manufacturer-neutral tool used for project engineering, parameterization, commissioning and monitoring of intelligent field devices and field components. It supplies diagnostic data, status data and parameter data to the Simatic PDM Maintenance Station, where the information is processed and supplemented by functionalities such as overview or work progress lists, overview, segment and detailed images, status logs, parameter data archiving, global and device-specific message lists as well as cyclical functions for reading out or exporting field device information.
The maintenance and servicing system is designed for use by small to medium-sized enterprises or production plants used for processes such as hybrid or biogas, wastewater treatment, painting lines in the automotive industry or paper manufacturing. The Simatic PMD Maintenance Station can also be used in specific plant sections. Version 2.0 of the Simatic PDM Maintenance Station can be used wherever intelligent field devices are in operation. The system is optimized for up to 500 field devices, and it is also possible to combine several Simatic PDM Maintenance Stations within one plant.
In production plants with Simatic automation stations, the Simatic PDM Maintenance Station is directly connected to the plant bus, and so communicates over the automation stations with the field devices of the lower-level field bus systems. In addition, a separate network can be created to the field devices if direct access is not possible.
The Simatic PDM Maintenance Station offers the same functionality and user guidance as the Simatic PCS 7 Maintenance Station, which is recommended for larger-scale applications using Simatic PCS 7 as a control system. "The special feature of the Simatic PDM Maintenance Station V 2.0 is that it can be used independently of Simatic PCS 7. Even if it isn't integrated into a Simatic PCS 7 project, it can use the existing infrastructure of a Simatic S7/PCS 7 project or create its own communication infrastructure," says Holger Rachut, Product Manager at Siemens. "It makes no difference how the field devices are connected, for instance using Profibus DP / PA, Profinet, HART or Ethernet," adds Rachut.
The compact Simatic PDM Maintenance Station is flexible and offers scope for expansion. It can even be used several times over within a single project for different tasks, for instance as a diagnostic station for sub-plants or a data collector for selected field devices. Used as a data collector, the Simatic PDM Maintenance Station enables the cyclical capture and transmission of identity, event and parameter data to the relevant data evaluation systems.
In its recommendation NE 107, Namur has defined four status signals to be used on a standardized basis for all field devices: device failure, maintenance required, out of specification and function check. This enables identical status visualization for all field devices based on what is known as the device description package DD/EDD, irrespective of type or manufacturer. The Simatic PDM Maintenance Station captures the diagnostic statuses and condition data of field devices implemented by the device manufacturer and described in DD/EDD. The maintenance station automatically reads this information from the field devices on a cyclical basis and where applicable signals any maintenance-related requirement, request or alarm on the basis of the NE 107, ensuring that service personnel are immediately informed and able to act or react promptly.
Development of the Simatic PDM Maintenance Station is based on Namur recommendations NE 105 in respect of field device integration, NE 107 for diagnostic status evaluation of field devices and NE 129 for general functionality of the device measurement station.
The Simatic PDM Maintenance Station requires only simple, low-cost engineering. Network structures and field devices can be simply adopted from existing projects. The basic package comprises a pre-installed industrial PC (Microbox IPC 427E) and the necessary function licenses, alongside a software recovery package. The Simatic PDM Maintenance Station can be optionally adapted within the quantity structure to the field devices to be monitored, and extended to include the server/client functionality of Simatic PDM.
For further information on the subject of Simatic PDM Maintenance Station, please see www.siemens.com/simatic-pdmms
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Evelyne Kadel
Siemens AG
Klaus-Bungert-Str. 6
40468 Düsseldorf
Germany
40468 Düsseldorf
Germany
+49 (211) 6916-1003