Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release17 February 2017Building TechnologiesZug
Desigo CC delivers new features for greater productivity, efficiency and transparency

The picture shows a part of the modular Desigo CC building management platform
State-of-the-art energy and power reports are now provided that give building operators complete transparency over energy distribution, power quality events and consumption in their buildings. This information can be used to initiate the measures needed to save costs as well as to increase system reliability.
Advanced reports filter complex data to provide the meaningful information and transparency that building operators need to make data-driven decisions. A new scripting function makes it possible to develop actions that can be executed automatically or manually in response to certain events. Additional storage supports not only long-term archiving of collected data but also the gathering of additional data, making Desigo CC suitable for even the most comprehensive applications.
For the first time, Desigo CC is now available in a special version for original equipment manufacturers (OEMs) which can be fully customized. The bandwidth of customizable features ranges from the user interface to adding disciplines and subsystems.
Finally, Desigo CC now has expanded migration tools that ease the switch from older-generation management systems to the state-of-the-art building management platform. Older versions of Desigo PX continue to be supported.
For further information on the Building Technologies Division, please see www.siemens.com/buildingtechnologies
For further information on Desigo CC, please see www.siemens.com/desigocc
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.