Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release13 April 2022Siemens AGZug,
Switzerland
Derichebourg Multiservices equips HQ with Siemens IoT sensors for energy efficiency

The Derichebourg Multiservices HQ in Créteil near Paris, France.
Derichebourg Multiservices is committed to using energy-saving
LED technology in its new headquarters; an architecturally significant building
resembling an inverted pyramid, built in 1970 and now upgraded with an
environmentally-focused approach.
The top three floors of the building, where
most of the open-plan offices are located, are equipped with 1,200 light
fixtures with Enlighted IoT sensors from Siemens. Wireless technology meant
they could be installed in just six weeks, and the lower floors will also be
upgraded in an expansion phase. Data from the sensors is continuously evaluated
to monitor and control energy consumption.
The project was implemented with the support
of lighting designer Le Studio Led, which integrates Enlighted sensors from
Siemens into its B2B lighting solutions, combining financial savings,
environmental friendliness and user satisfaction. In the tertiary sector,
lighting often accounts for 10 to 15 percent of total energy consumption.
“The data collected by our Enlighted sensors
is hugely valuable in improving the energy efficiency of buildings, and also the
comfort and productivity of the people who work in them,” said Stefan Schwab,
CEO of Enlighted. “We are pleased to be working with both Le Studio Led and
Derichebourg Multiservices
to develop new use cases, which will allow for the optimization of services for
occupants.”
Added value for Derichebourg Multiservices and its customers
The collected data provides a wealth of
information, making it possible to detect changes in environmental conditions
and room occupancy, and to respond in real time.
In addition to using the IoT sensors for
reducing its own energy consumption, Derichebourg Multiservices also intends to use the data for
additional applications in the future, demonstrating the practical benefits to
customers and offering them related new services. In cooperation with Le Studio
Led and Siemens, Derichebourg Multiservices is working to develop new use cases to optimize
services in buildings, with the intention to integrate them into its service
offering. For example, occupancy data from the sensors can be used to schedule
cleaning services in buildings based on actual demand. The data could also be
used to optimize the reception of guests to the building, improve comfort
levels or even strengthen on-site security.
“As part of our service delivery activities,
the breadth of possibilities offered by IoT sensors represents a tremendous
development opportunity,” said Silvine Thoma, Communications Manager for
Derichebourg Multiservices.
“Not only do we act on our own consumption, but we also benefit from a
real-world showcase of their usage, in order to offer additional services to
our customers, for our remote monitoring or cleaning activities, for example.”
For more information about Siemens Smart
Infrastructure, see
www.siemens.com/smartinfrastructure
www.siemens.com/smartinfrastructure
For this press release
Follow us on Twitter
Siemens Smart Infrastructure (SI) is shaping the market for intelligent, adaptive infrastructure for today and the future. It addresses the pressing challenges of urbanization and climate change by connecting energy systems, buildings and industries. SI provides customers with a comprehensive end-to-end portfolio from a single source – with products, systems, solutions and services from the point of power generation all the way to consumption. With an increasingly digitalized ecosystem, it helps customers thrive and communities progress while contributing toward protecting the planet. Siemens Smart Infrastructure has its global headquarters in Zug, Switzerland. As of September 30, 2021, the business had around 70,400 employees worldwide.
Siemens AG (Berlin and Munich) is a technology company focused on industry, infrastructure, transport, and healthcare. From more resource-efficient factories, resilient supply chains, and smarter buildings and grids, to cleaner and more comfortable transportation as well as advanced healthcare, the company creates technology with purpose adding real value for customers. By combining the real and the digital worlds, Siemens empowers its customers to transform their industries and markets, helping them to transform the everyday for billions of people. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a globally leading medical technology provider shaping the future of healthcare. In addition, Siemens holds a minority stake in Siemens Energy, a global leader in the transmission and generation of electrical power.
In fiscal 2021, which ended on September 30, 2021, the Siemens Group generated revenue of €62.3 billion and net income of €6.7 billion. As of September 30, 2021, the company had around 303,000 employees worldwide. Further information is available on the Internet at
www.siemens.com.
Reference Number: HQCOPR202204126431EN