Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release03 July 2018Process Industries and DrivesNuremberg
Cost effective compact IEEE 1588 Ethernet switches for reduced downtimes

The picture shows the Ethernet switches Ruggedcom RSG908C and Ruggedcom RSG910C.
Tested and certified to withstand extreme temperature, vibration and shock, the Ruggedcom RSG908C and RSG910C offer exceptional reliability for industrial applications that require high bandwidths and accommodate future network expansions. Both devices offer either a 24/48 VDC (10 – 60 VDC) power supply or a high voltage (85 – 264 VAC / 88 – 300 VDC) power supply depending on the ordered configuration. They can also be ordered with conformal coating.
The Ruggedcom RSG908C has a total of 8-ports including 4 Gigabit SFP ports providing ultimate flexibility in media and distance. It can connect up to 4 devices (e.g. IEDs) via its 100BASE-FX LC ports.
The Ruggedcom RSG908C has a total of 8-ports including 4 Gigabit SFP ports providing ultimate flexibility in media and distance. It can connect up to 4 devices (e.g. IEDs) via its 100BASE-FX LC ports.
The Ruggedcom RSG910C has a total of 10-ports including 4 Gigabit SFP ports. It can connect up to 6 devices (e.g. IEDs) via its 10/100/1000BASE-T RJ45 ports. The Ruggedcom RSG908C and the RSG910C received a Red Dot Award in 2018 in the industrial design category. The products were recognized for their innovative industrial design representing a modular compact enclosure that allows high performance technology to operate at extreme temperatures while at the same time enabling easy and time saving installation in small cabinets and panels.
The Ruggedcom RSG908C and Ruggedcom RSG910C can be used for precise time synchronization in Electric Power industry; for high-bandwidth applications such as video streaming in Transportation industry, and for time-critical applications such as drilling automation, SCADA (Supervisory Control and Data Acquisition) and RTU (Remote terminal unit) solutions for wellhead automation, pipeline monitoring, compression or pumping stations in the oil & gas industry.
More information is available at www.siemens.com/rsg900c
For this press release
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world'''s largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 377,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
David Petry
Siemens AG
Werner-von-Siemens-Str. 65
91052 Erlangen
Germany
91052 Erlangen
Germany
+49 (9131) 7-26616