Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release15 July 2020Digital IndustriesNuremberg
Bringing intelligence to the shop floor with Siemens Industrial Edge
With Siemens Industrial Edge, Siemens offers users the opportunity to close the gap between conventional local data processing and Cloud-based data processing, depending on individual requirements. With Edge computing, large volumes of data can be processed locally almost in real time. Siemens provides users with a broad spectrum of applications for this, including data processing, data visualization via web server, data transmission to the Cloud or IT infrastructure and fast innovation cycles for app development. In addition, storage and transmission costs are reduced for users because large volumes of data are preprocessed, and only relevant data is then transmitted to a Cloud or IT infrastructure. Siemens Industrial Edge supports Cloud transmission protocols for Mindsphere, the open, cloud-based operating system from Siemens as well as Message Queuing Telemetry Transport (MQTT). This makes data transmission secure and effective.
Siemens Industrial Edge: Industrial Edge Management, Edge devices, Edge apps
Siemens Industrial Edge comprises the Industrial
Edge Management System, Edge devices and Edge apps. The Industrial Edge
Management System can be used to manage all connected Edge devices centrally and
to monitor their condition. In addition, Edge apps are always distributed to
Industrial Edge devices efficiently and securely in the latest version. Applications
can be installed on Edge devices regardless of the machine operating state
without adverse effects. Apps for Siemens Industrial Edge can be provided both
by Siemens and by third-party providers. This means that users and machine
builders also have the opportunity to develop their own applications, which are
tailored to the individual requirements of their machines.
With the acquisition of US startup Pixeom, Siemens has obtained components
for Edge Runtime for applications as well as for Device Management as part of
the Siemens Industrial Edge ecosystem. The technology developed by Pixeom based
on the Docker IT standard offers open interfaces e.g. for connection to the Mindsphere
App Store, for the management of third-party hardware and for the creation of apps
by Siemens customers. The Edge apps are offered via a marketplace in Mindsphere.
The operating system of Siemens Industrial Edge is integrated in a universal
security concept. It enables the stable operation of one or more apps in
parallel and also ensures a protected software environment for the execution of
applications on Edge devices.

Maximum flexibility and productivity for manufacturing plants across the entire life cycle
Industrial
Edge with Simatic offers Siemens users a platform that can meet the challenges
of today and tomorrow. Automation components such as Simatic controllers are additionally
supported by Edge devices, enabling larger volumes of plant data to be
processed profitably and providing vital information for the continuous
improvement of productivity. At the same time, new applications such as condition
monitoring or predictive maintenance are gaining ground in conventional automation
technology. Furthermore, Edge computing offers a previously unattainable level
of flexibility: plants can be kept up to date at all times via functional, feedback-free
updates even for the plant life cycles expected in automation. Siemens users
are supported in application development with frameworks and access to integrated
connectivity with the world of automation. So far, the following Edge applications
are being presented for Simatic Edge:
- Simatic Notifier
- Simatic Assistant for Machines
Stable processes and increased productivity for machine tools
For machine
tools, Industrial Edge with Sinumerik provides a machine-based platform for software
apps, which captures, preprocesses and analyzes high-frequency data from the
machine tool. In addition, complex tool paths can be calculated, and
non-productive times or work area monitoring can be optimized. With Sinumerik
Edge, Siemens enables machine tool users to improve workpiece and process quality,
to increase machine availability and to further optimize machine processes. The
following Edge apps have been presented for Sinumerik Edge:
For workpiece
quality:
- Analyze MyWorkpiece /Capture
- Analyze MyWorkpiece /Toolpath
- Analyze MyWorkpiece /Monitor
- Analyze MyWorkpiece /Vision (AI-based)
For performance
optimization:
- Optimize MyMachining /Magazine (AI-based)
- Optimize MyMachining /Trochoidal
For condition monitoring and process stability:
- Protect MyMachine /3D Twin
- Analyze MyMachine /Condition
More intelligence for drive systems
Siemens is currently also piloting the connection of a Sinamics drive
system to the Siemens Industrial Edge platform. This will enable high-frequency
data exchange with an Edge device in drive technology in the future. The
connection of Sinamics frequency converters to an Edge device enables users of
machines and applications to perform complex analyses of data that is already
collected in the drive. Machine-learning algorithms identify patterns and
detect anomalies and their causes, thus providing timely indications of any
pending maintenance. This minimizes downtimes and reduces the consumption of
resources. In the field of intralogistics, for example, conclusions can be made
about the current belt tension in a storage and retrieval machine. The belts,
which are driven by the motor and frequency converter, require a specific
tension to ensure that the application runs smoothly. If the visualization of
the data analyses shows irregularities in the drive system, maintenance of the
belt can be initiated in a timely manner, for example.
For further
information regarding Siemens Industrial Edge, please see
www.siemens.com/industrial-edge
www.siemens.com/industrial-edge
For this press release
Siemens Digital Industries (DI) is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI’s unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has around 76,000 employees internationally.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of intelligent infrastructure for buildings and distributed energy systems, and automation and digitalization in the process and manufacturing industries. Through the separately managed companies Siemens Energy, the global energy business of Siemens, and Siemens Mobility, a leading supplier of smart mobility solutions for rail and road transport, Siemens is shaping the energy systems of today and tomorrow as well as the world market for passenger and freight services. Due to its majority stakes in the publicly listed companies Siemens Healthineers AG and Siemens Gamesa Renewable Energy (as part of Siemens Energy), Siemens is also a world-leading supplier of medical technology and digital healthcare services as well as environmentally friendly solutions for onshore and offshore wind power generation. In fiscal 2019, which ended on September 30, 2019, Siemens generated revenue of €86.8 billion and net income of €5.6 billion. At the end of September 2019, the company had around 385,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Reference Number: HQDIPR202007135939EN
Contact
Andreas Friedrich
Digital Industries - Industrial Edge
Gleiwitzer Str. 555
90475 Nuremberg
Germany
90475 Nuremberg
Germany
+49 (1522) 2103967
Katharina Lamsa
Digital Industries - Sinumerik Edge
Gleiwitzer Str. 555
90475 Nuremberg
Germany
90475 Nuremberg
Germany
+49 (172) 8413539