[{"name":"Home","site_name":"Press | Company | Siemens","description":"","url_str":"\/global\/","level":0,"image":"","base_root":"https:\/\/press.siemens.com","base_nid":"5","base_nodepath":"\/node\/5","base_path":"\/global\/","base_secure_url":"https:\/\/press.siemens.com\/global","children":null}]
[]
Please use another Browser
It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and
usability.
For the best experience we suggest that you download the newest version of a supported browser:
Simatic HMI Thin Client Ex OG in IP66 for use in the chemical, oil, gas and shipbuilding industries
Siemens has extended its system family of all-round protected HMI (Human Machine Interface) devices for machine-related, cabinet-free visualization and automation. High-performance Simatic Thin Client PRO operator terminals with 15, 19 and 22 inch screen sizes and all-round IP65 degree of protection are new to the range. Like all devices in the PRO series, the new Thin Clients can be extended by mountable components (extension units) – such as mounting adapter, keyboard tray and keyboard. New expansion options are operator controls with USB interfaces and an extension box with adjustable handles for easy operation of the panels on the machine.
Simatic HMI Thin Client PRO operator terminals with IP65 degree of protection and 15, 19 and 22 inch screen sizes
Simatic HMI Thin Client Ex OG in IP66 for use in the chemical, oil, gas and shipbuilding industries
Siemens has extended its system family of all-round protected HMI (Human Machine Interface) devices for machine-related, cabinet-free visualization and automation. High-performance Simatic Thin Client PRO operator terminals with 15, 19 and 22 inch screen sizes and all-round IP65 degree of protection are new to the range. Like all devices in the PRO series, the new Thin Clients can be extended by mountable components (extension units) – such as mounting adapter, keyboard tray and keyboard. New expansion options are operator controls with USB interfaces and an extension box with adjustable handles for easy operation of the panels on the machine.
The picture shows the Simatic Thin Client PRO operator terminal.
The picture shows the Simatic HMI Thin Client Ex OG.
The all-round IP66 protected Simatic HMI Thin Client Ex OG is the new addition to the series of Ex HMI devices. It can be used in 1/21 and 2/22 zones without any special measures such as elaborate enclosures or additional certifications. The Ex OG HMI devices are specially designed for applications in industries such as chemicals, oil, gas and shipbuilding, and are suitable for use in extreme temperatures ranging from -40 C to +65 degrees Celsius.
The new Ex OG devices are complemented by material for four mounting types and equipment options such as cameras, Bluetooth, wireless and internal RFID(Radio Frequency Identification) readers.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 377,000 employees worldwide. Further information is available on the Internet at www.siemens.com.