The need for electromobility is growing, as is the need for an efficient charging infrastructure. As a pioneer in electromobility, Siemens has global experience, maintains a strong portfolio along the entire value chain, and plays an active role in advancing the development and standardization of charging solutions worldwide.Siemens is part of the "FastCharge" research project together with BMW Group as consortium leader, Allego GmbH, Phoenix Contact E-Mobility GmbH as well as Dr. Ing. h.c. F. Porsche AG. This project is investigating the technological requirements that vehicles and infrastructure must meet in order to be able to use extremely high charging capacities. The industrial companies involved in the research project presented the latest advancements in the field of fast and convenient energy supply for electrically powered vehicles on December 12, 2018. The prototype of a charging station with a capacity of up to 450 kW was inaugurated in Jettingen-Scheppach, Bavaria. At this ultra-fast charging station, electrically powered research vehicles created as part of the project are able to demonstrate charging times of less than three minutes for the first 100 kilometres of range or 15 minutes for a full charge (10-80 % State of Charge (SOC)).The energy supply system of Siemens used in the project contains both high-power electronics for the charging connections as well as the communication interface to the electric vehicles. For the connection to the public power grid, a charging container was implemented with two charging connections for CCS-compatible vehicles. One connection has an unprecedented charging capacity of max. 450 kW while the second can deliver up to 175 kW.
- Siemens successfully completed the first phase of its shallow water test of the Subsea Power Grid.
- The development program was conducted in collaboration with industry partners Chevron, Equinor, ExxonMobil, and Eni Norge.
- This will be the world's first Subsea Power Grid for medium voltage power distribution using pressure compensated technology.
Siemens has successfully concluded the first phase of its Subsea Power Grid shallow water test in Trondheim, Norway. Siemens, in collaboration with industry partners Chevron, Equinor, ExxonMobil, and Eni Norge, is in the final stages of a program to develop a barrier-breaking system that will become the world’s first Subsea Power Grid designed for distribution of medium voltage power using pressure compensated technology.
With the DynaGridCenter project, Siemens worked alongside partners in science and research to develop the next generation of grid control centers. For the first time, assistant systems visualize dynamic processes that bring the energy transition to the power grid and provide targeted recommendations for actions to optimize the grids and prevent blackouts.
Siemens Building Technologies Division is acquiring Building Robotics Inc., a market leader in the fast growing digital workplace experience app domain. The simple-to-use app Comfy enables people to take control of their environment and provides feedback on their space. With this acquisition, Siemens is setting a further milestone in smart building solutions.