- Siemens will supply four 400 kV HVDC transformers for cross-channel link
- Efficient 2,000 MW power transmission link between France and the UK will supply up to 3 million homes with electricity
Siemens will deliver four transformers, each with a capacity of 400 kilovolts (kV) and 315 megavolt amperes (MVA), on behalf of the British grid operator National Grid. The grid operator will replace the old transformers in the high-voltage direct-current (HVDC) cross-channel link. The new transformers are quieter, have lower transmission losses and will significantly improve the system's reliability. The HVDC link connects France and England and makes it possible to efficiently exchange energy in both directions. The order includes the supply, installation and commissioning of the transformers for the Sellindge converter station in England. Siemens will complete the work by mid-2019.
Siemens has received an order from the regional grid operator EWE Netz GmbH to supply the key components of a Siharbor shore power supply system in Cuxhaven. The order includes the complete transformer station as well as the cable feed system for ro-ro (roll-on/roll-off) ships. The plant owner will be the northern German Gesellschaft für Hafeninfrastruktur Niedersachsen Ports (NPorts). With a power output of 630 kilowatts (kW), the plant will supply these ships with electricity during their lay time. They will thus be able to turn off their diesel generators, significantly lowering exhaust gas and noise pollution. The berth is located next to the new factory for wind turbines operated by Siemens Gamesa, which will be the plant's main user in the future. Siemens Gamesa will ship wind turbine components to its sister factory in Hull, UK. The Siharbor system is expected to go into operation by April 2018.