- Monitoring of all 3-phase grids from 200 V to 690 V nominal voltage
- Frequency monitoring from 15-70 Hz for more detailed information
- IO-Link enables transmission and evaluation of measured values in the
controller or higher-level systems
- Certification according to SIL 1 (IEC 62061) and PL c (EN ISO 13849-1)
standards for a wide range of applications
Siemens has launched a new generation of line monitoring relays. The SIRIUS 3UG5 line monitoring relays combine proven technology with new functions and applications. The relays are the easiest way to monitor standards-compliant grid stability and quality, ensuring proper system operation and a long service life of components such as motors or compressors. Grid monitoring relays are used in critical areas such as hospitals or the process industry, which require a high-quality, fail-safe supply of power. Other areas of application include cranes, elevators, air, and air-conditioning compressors, as well as the timber industry.
-
90 new trains in size XXL
- For the first time, all cars are completely integrated and set new standards
with a train length of over 200 meters
- Financing guaranteed by
the State of Bavaria
Passengers on Munich’s S-Bahn can soon look
forward to traveling on the most modern S-Bahn trains in Germany. Siemens
Mobility will deliver 90 superlative new S-Bahn trains worth more than two
billion euros after winning an EU-wide tender. The contract includes an option
for additional trains. Financing for the trains is guaranteed by the State of
Bavaria through a leasing model.
- 15 additional Vectron AC and Vectron MS
locomotives
- Delivery includes locomotives with a top speed
of 200 km/h
- Milestone reached: 100 Vectrons ordered by
Akiem since 2021
Akiem, a leading European
rolling stock leasing company, has ordered an additional 15 Vectron AC and
Vectron MS locomotives from Siemens Mobility. The order was placed as part of a
framework agreement for the purchase of locomotives that was signed in December
2021. Locomotives from this new call will be delivered between 2025 and 2027.
Akiem previously ordered 20 Vectron locomotives from Siemens Mobility in December
2021 and an additional 65 units last August.
- In a pilot project, Siemens is combining its Sigreen emissions management software with BayWa Carbon Connect, BayWa’s software for emissions offsetting
- The real carbon footprint of products is made transparent across the supply chain, from emission generation and reduction to offsetting
- In an initial use case, Siemens is offsetting the carbon emissions of selected products of the Simatic S7-1500 family at the Electronics Works Amberg for the duration of the project
The technology company Siemens and BayWa AG are working together to advance CO2-optimized industrial production. As part of a pilot project, the two companies are combining Sigreen, Siemens’ software for emissions management, with BayWa Carbon Connect, BayWa’s software for emissions offsetting.
- Delivery of 15 Vectron MS locomotives
- MSC subsidiary MEDWAY Belgium NV will take
delivery of equipment and is a new customer of Siemens Mobility
- Locomotives can operate in 12 European
countries
Siemens
Mobility has received an order from MSC subsidiary MEDWAY Belgium NV for 15 Vectron
MS locomotives. MEDWAY plans to use the locomotives for cross-border freight
transport in Europe and also for supplementing container transport by ship in
serving the eastern hinterland of Antwerp.
- Industrial Connectivity Lab opens at the Erlangen site
- Test environment for industrial connectivity technologies
- 5G, WLAN, RTLS, and RFID: Users test application scenarios and interoperability in industrial conditions
The technology company Siemens has opened a new test laboratory for industrial connectivity technologies at its Erlangen site. Embedded in the Siemens Technology Center on the Erlangen campus, the Industrial Connectivity Lab offers 300 square meters of space for extensive testing of any connectivity solution in industrial environments: Industrial WLAN, 5G, real-time localization systems (RTLS), and radio frequency identification (RFID).
City of Hamburg, Deutsche Bahn, and Siemens
Mobility sign cooperation agreement for Digitale S-Bahn Hamburg 2.0
New
intelligent operations control system to be tested until UITP Congress 2025
Partners jointly invest 35 million euros
(Hamburg, July 18,
2023) With the Digitale S-Bahn Hamburg, train travel will become even more
environmentally friendly in the future. Deutsche Bahn (DB), the city of
Hamburg, and Siemens Mobility are introducing a new intelligent operations
control system for the Digitale S-Bahn in Hamburg, aiming to reduce the trains'
power consumption by up to 30 percent. The system will be tested until the UITP
World Congress 2025. The project, costing 35 million euros, is jointly funded
by DB, the city of Hamburg, and Siemens Mobility. A cooperation agreement for
the Digitale S-Bahn Hamburg 2.0 was signed by representatives of the partners
today.
- Innovative Sentron 3WA circuit breaker series part of Siemens Xcelerator
- Designed to improve ease of use, reliability, and digitalization when integrating into existing systems
- Essential for critical infrastructure, such as hospitals or data centers
- 3WA1 (IEC), 3WA2 (UL489), and 3WA3 (UL1066+IEC) offer worldwide compatibility
Siemens has launched two new additional
versions of its innovative Sentron 3WA Power Circuit Breakers, alternatively
known as Air Circuit Breakers (ACBs). Series 3WA3 meets the requirements of UL
1066 and IEC 60947-2 standards, which enables customers to use it worldwide.
This is particularly advantageous for switchgear manufacturers and OEMs producing
systems for both standardization areas – IEC and UL. The 3WA2 series is
designed exclusively for the UL 489 market. The two new ACB model series
complement the 3WA1 version for IEC markets, which has been launched in the
fall of 2020. Siemens offers a full range of ACBs which are based on a
consistent system and offer great flexibility for applications around the
globe. The Sentron 3WA Power Circuit Breakers are part of the Siemens
Xcelerator portfolio. Siemens Xcelerator is an open digital business platform
that enables customers to accelerate their digital transformation easier,
faster, and at scale.
- Independent analyst firm has recognized Siemens Smart Infrastructure as a leader in integrated smart building security software
- The software is part of the Siemens Xcelerator portfolio
Industry analyst firm Verdantix has ranked Siemens Smart Infrastructure as one of the leading providers for security software in smart buildings. Their recently published “Green Quadrant: Integrated Smart Building Security Software 2023” report analyzes and evaluates ten companies that are shaping the market. Verdantix noted that Siemens solutions offer highly advanced unified security management capabilities. The assessed Siemens software is part of Siemens Xcelerator, an open digital platform that enables customers to accelerate their digital transformation.
- Maintenance for Vectron locomotives over a
period of 15 years
- Cloud-based Railigent X applications to ensure
efficient maintenance processes
Alpha Trains, the
leading locomotive and trains lessor in Europe, has awarded Siemens Mobility a
long-term service and maintenance contract. The contract covers the complete
maintenance of Vectron locomotives over a period of 15 years, including revisions
at the Siemens Rail Service Center in Munich-Allach. Maintenance of the
locomotives will be tailored to their operation and carried out as needed in
thirteen different countries at the Siemens Mobility Service facilities located
along the major trans-European rail corridors.