- Siemens will refurbish 30-year-old HVDC back-to-back system in the State of Madhya Pradesh in India
- Modernization will extend the lifetime to ensure reliable power supply
- First Siemens refurbishment project of a third-party HVDC system
Power Grid Corporation of India (POWERGRID), the Central Transmission Utility of India, has chosen Siemens to modernize the country's first and oldest high voltage direct current (HVDC) link, Vindhyachal. Located in the central Indian state of Madhya Pradesh, the 500-megawatt HVDC back-to-back system was put into operation in 1989 to interconnect the asynchronous 400-kilovolt alternating current networks of the Northern and Western regions. By installing its latest HVDC components Siemens will extend the useful life of the link. This will be the first Siemens HVDC modernization project in India and globally the company's first refurbishment of a third-party system involving replacement of the thyristor valves. The upgrade is expected to be completed in 2021.
Arja Talakar has been appointed CEO of Siemens Oil & Gas, effective April 1, 2019. He will be based in Houston, Texas, the global headquarters for Oil & Gas and its parent operating company, Siemens Gas and Power.
- Siemens will supply three Dresser-Rand® 5HHE-VL-3NL reciprocating compressors for what will become the largest hydrogen production unit in the United States.
A leading industrial gas company recently selected Siemens to supply three Dresser-Rand® 5HHE-VL-NL reciprocating compressors for a new, state-of-the-art steam methane reformer (SMR) in Texas. The SMR will provide high-purity hydrogen for the gas company’s customers throughout the region.
- Siemens' broad energy portfolio and services will help ensure long-term reliability and efficient operations
- Integrated, redundant plant design features two SGT-600 gas turbines with DLE technology running on residue gas with high concentrations of hydrogen
- Project highlights the integrated value of Siemens Gas and Power
Braskem, the largest petrochemical company in Latin America, recently entered into an agreement with Siemens to modernize a cogeneration power and steam plant at its Petrochemical Complex in Sao Paulo, Brazil. Completion of the project is expected in early 2021.
- 1.3-gigawatt turnkey combined cycle power plant
- Long-term service program and operation & maintenance (O&M) services included
- Largest LNG-to-power development in Latin America
- Total project volume of €1 billion
Siemens has secured an order for the turnkey construction of a new combined cycle power plant for the integrated LNG-to-Power project GNA 1 of Gás Natural Açu in the Port of Açu in the state of Rio de Janeiro, Brazil. Siemens is providing an equity investment and owns one-third of the project company Gás Natural Açu (GNA) together with Brazil logistics company Prumo Logística S.A. and BP. In addition, Siemens signed a long-term service agreement and will operate and maintain the plant to help ensure reliability, availability and operational performance. The order is the first application for the highly efficient and proven Siemens H-class gas turbine in Brazil. With a capacity of approximately 1.3 gigawatts (GW), the power plant will provide affordable and clean energy for Brazil. Total project volume for GNA 1 is approximately €1 billion (R$4.5 billion).
- Services support first use of Siemens H-class turbine in an aluminum smelting facility globally
- Siemens' first long-term service agreement in the UAE for an H-class turbine
- Power services will ensure reliable operations for stable power production
Emirates Global Aluminum (EGA), the world's largest 'premium aluminum' producer, and Siemens announced the first power services agreement for an H-class gas turbine in the United Arab Emirates (UAE). With the new 20-year service agreement, Siemens will provide maintenance and repairs as well as onsite personnel support for the gas turbine and its generator at the planned over 600-megawatt (MW) combined cycle project feeding EGA's Jebel Ali power plant in Dubai.
- SensgearTM technology launch for digital connectivity of switchgear products
- New Sensformer® advanced with applications based on digital twin simulation of transformers
- Portfolio extension comes with comprehensive data analytics for added transparency, enhanced productivity, and advanced intelligence
Siemens is introducing Sensgear, its new digital switchgear portfolio, and the Sensformer advanced at this year's Hannover Messe. With the combination of the already well-established digitally connected transformer, the Sensformer, and the new Sensgear technology, all substation transmission assets are now fully connective, allowing operators to check their status via online applications in real time. Gas-insulated switchgear, circuit breakers, surge arresters, disconnectors, instrument transformers, and coil products will henceforth be equipped with Sensgear technology. All devices are connected via a smart and robust Internet of Things (IoT) gateway that securely transmits the required information to a cloud-based storage and visualization platform. All Sensgear products provide additional transparency with GPS and local weather information as well as product-specific measurement data that includes gas density, liquid temperature, gas leakage, and switching position.
- Simatic PCS 7 Plant Automation Accelerator V3.0 plant and automation engineering software closes the gap between plant engineering and the process control system
- More powerful, more open version
- Increased system openness based on GSDML and NE150 standards
- Seamless engineering through the integration of various Simatic components
Siemens has extended its engineering software for planners and automation engineers, Simatic PCS 7 Plant Automation Accelerator 3.0 (PAA), to include new functions for even more flexible and integrated automation engineering. With this latest software version, Simatic PCS 7 automation projects can be configured even more easily and efficiently. With Version 3, the PAA software closes the gap between plant engineering and the process control system. The entire plant structure including measuring point data can be generated easily and synchronized between the systems. Automation engineers are supported in all phases from tender preparation (such as bills of material), automatically generated process control data from electrical engineering in the Siemens Simatic PCS 7 process control system (including controlled mass data engineering), to as-is documentation of the process automation.
- New Edge functionality provides better and more secure access to remote data
- Simplified integration of engineering data
- HTML5-based, new web browser client
- Server virtualization support increases efficiency and performance
Siemens launches the new release V 6.0 of their flagship XHQ Operations Intelligence with enhanced performance while increasing the overall usability at the same time. With the new version, users benefit from numerous enhancements such as edge functionality. With an end-to-end secured site integration and light weight installation, this provides easy and secure access to remote/distributed data from all production (operation) and enterprise levels. The new version also enables enhanced operations by simplifying the integration of engineering data: interfaces with Siemens or third party solutions, such as Comos, Comos Walkinside, PlantSight, Teamcenter and more, are now improved and easily integrated into the system. In addition, the new HTML5-based web browser client is compatible with existing solutions. Version 6.0 no longer requires a Java browser plug-in (Java applet) for the full desktop environment, i.e. can run as a HTML5 compatible browser solution. Server virtualization support is available, which enables multiple operating systems to run on a single physical server. This increases business efficiency and overall performance.