- Latin America’s first fully automated metro line (GoA 4)
- Siemens Mobility digitalized CBTC technology installed across entire 15 km of track,11 stations, and 29 trains
- Automated signaling provides greater availability, enhanced operations, and passenger experience
ViaQuatro has successfully begun full operation of São Paulo’s entire Metro Line 4 with Siemens Mobility’s Communications-Based Train Control (CBTC) signaling. Since its first stretch opened in 2010, it has been the first fully automated metro line in South America that can operate with GoA 4, the highest grade of automation that allows trains to be automatically controlled and operated. The digitalized and optimized system allows for a more efficient and centralized control of operations, while also increasing the safety, availability, and capacity across the entire network.
Siemens Mobility has handed over the 100th ICE
4 to Deutsche Bahn. The train was christened “Rheinland-Pfalz” at the official
ceremony held in Mainz today, attended by Dr. Richard Lutz, CEO of Deutsche
Bahn AG, Dr. Michael Peterson, DB Board Member for Long Distance Passenger
Transport, Dr. Volker Wissing, Federal Minister for Digital Affairs and
Transport, Malu Dreyer, Minister President of Rhineland-Palatinate, and Dr.
Roland Busch, CEO of Siemens AG.
“We are pleased that the ICE 4 is the backbone of DB’s long-distance transport and thank our customer for their trust. Our trains help DB make rail transport more attractive and protect the environment. The fact that we have delivered 100 ICE 4s shows that we have the right portfolio for high-speed transport. Moreover, the ICE secures thousands of jobs in Germany,” said Roland Busch, CEO of Siemens AG.
DB will receive a total of 137 ICE 4 trains in various configurations by the end of 2024. In addition to the 50 12-car trains that have already been delivered, 19 of the 37 ordered 7-car trains are already in use, such as on the ICE line between Cologne and Berlin. 33 13-car XXL ICE trains, of which DB has ordered 50, have also been added to the fleet since February 2021. The 13-car trains have almost 1,000 seats, more than ever before in an ICE and five times more than in a medium-haul airplane. Siemens Mobility delivers a new ICE 4 every three weeks. At this rate, DB will be able to expand its capacity by another 11,000 ICE 4 seats by the end of this year.
Siemens Mobility's Vectron locomotives are used for both freight and passenger service. During the development of the locomotive, the focus was on providing a future-proof design, investment security, environmental compatibility, fungibility, retrofitting capability and convertibility. The Vectron can be delivered as a purely electrical version for operating with alternating current (AC) or direct current (DC) power systems as well as a multisystem (MS) variant in the power classes 5.2 MW, 5.6 MW and 6.4 MW. Along with the desired national train control system, the locomotives can also be equipped with the latest European Train Control System (ETCS). The locomotives are built in the Siemens Mobility plant in Munich-Allach, Germany. For freight transport in Germany, Siemens Mobility also offers the Smartron standard locomotive and the Vectron Dual Mode, a combination of diesel and electric locomotive.
- Siemens Mobility delivers Vectron AC locomotives
- Contract includes maintenance for eight years
Reichmuth & Co Investment Management AG has ordered 35 Vectron AC locomotives from Siemens Mobility through its investment vehicle LokRoll 3 AG. LokRoll 3 will lease the locomotives to SBB Cargo for eight years through its asset manager Northrail GmbH, which it commissioned for the deal. The entire transaction was arranged and structured by Paribus Rail Investment Management GmbH. The lease also includes local maintenance of the locomotives by Siemens Mobility for eight years. The Vectrons will be manufactured at the Siemens Mobility plant in Munich-Allach and delivered in 2024.
Siemens Mobility GmbH achieved the ISO 27001 certification on July 1, 2022. The ISO 27001 certification encompasses 20 Siemens Mobility locations in Germany with more than 9,000 employees and involves Siemens Mobility Business Units, such as Rolling Stock, Rail Infrastructure, Turnkey Systems and Customer Services and all disciplines, including procurement, development, production and project management. ISO 27001 is an internationally acknowledged standard specifying cybersecurity requirements that organizations must fulfill and to which they must adapt. Increasing digitalization brings benefits – as well as the need for adequate protection against cyberattacks. Rail operators face new cyber threats and cyber laws are giving rise to new requirements. Siemens Mobility offers secured products and solutions that are integrated into one holistic security architecture and provide security services. With these, Siemens Mobility secures rail systems from end to end throughout the complete lifecycle. The ISO 27001 certification is another building block in the protection of the entire development and production lifecycle for mobility systems. The ISO 27001 certification is a milestone for Siemens Mobility on the way to digitising the rail industry.
- First order for multisystem locomotives with XLoad equipment package
- XLoad enables significantly higher trailer loads
- Contract includes locomotives and their maintenance
Switzerland’s SBB Cargo International AG, in cooperation with SüdLeasing GmbH, has ordered 20 Vectron multisystem locomotives equipped with the XLoad package from Siemens Mobility. SBB Cargo International will lease the locomotives from SüdLeasing under a long-term rental plan with a flexible term. The contract also includes maintenance of the locomotives by Siemens Mobility. Vectron XLoad is an equipment package developed to improve traction performance and increase trailer loads. With this XLoad option, for example, operators on the North-South Corridor will be able to use only one rather than two four-axle locomotives for a train. The Vectrons are designed for a maximum operating speed of 160 km/h. The locomotives will be delivered beginning in 2024.
- Siemens completes sale of mail and
parcel business to Körber
- Further step in simplifying Siemens’
portfolio achieved
The sale of
Siemens Logistics’ mail and parcel business to the Körber Group closed
successfully on July 1. In February 2022, Siemens had announced the
contract signing for the sale of the mail and parcel business to the Körber
Group for €1.15 billion (enterprise value).
Magdeburg/Brandenburg an der Havel, June 30, 2022
– Today Ostdeutsche Eisenbahn
GmbH (ODEG), together with representatives from the states of Mecklenburg-Western
Pomerania, Berlin, Brandenburg and Saxony-Anhalt and the transport authorities VBB-Verkehrsverbund Berlin-Brandenburg GmbH,
Nahverkehrsservice Sachsen-Anhalt GmbH, and Verkehrsgesellschaft
Mecklenburg-Vorpommern mbH, signed the transport contract for the Elbe-Spree
network in Brandenburg an der Havel. As part of the ceremony, one of
the new six-car Desiro HC trains was presented in Magdeburg and Brandenburg an
der Havel by train manufacturer Siemens Mobility GmbH.
- Atlantia S.p.A. finalizes the
acquisition of Yunex Traffic from Siemens Mobility for €950 million
Siemens Mobility has successfully
completed the sale of Yunex Traffic to Atlantia S.p.A. for €950 million. In
January 2022, Siemens had announced the contract signing to sell the Intelligent Road Infrastructure and Traffic Solutions
Business to Atlantia S.p.A. Following the required
approvals by the relevant authorities, the transaction has closed as of
June 30, 2022.
- Siemens Mobility is building seven two-car Mireo Plus H trains powered by fuel cells for Niederbarnimer Eisenbahn (NEB)
- Switching from diesel to hydrogen on the Heidekrautbahn will reduce annual CO₂ emissions by around three million kilos and save 1.1 million liters of diesel
- For Siemens Mobility the first order for a fleet of trains based on hydrogen technology
- The hydrogen fleet will be delivered in the fall of 2024. The trains are planned to operate on the Heidekrautbahn network (RB27) beginning in December 2024.
- The order placed with Siemens Mobility also includes a service and spare parts supply agreement (TSSSA) covering the entire term of the transport contract.
Siemens Mobility has been commissioned by Niederbarnimer Eisenbahn (NEB) to deliver seven two-car Mireo Plus H trains for the Heidekrautbahn network (RB27) in the Berlin-Brandenburg metropolitan region. Equipped with a fuel cell drive system and a lithium-ion battery, this second-generation hydrogen train provides completely CO₂ emission-free mobility.