- Industry
analyst firm recognizes Siemens for clear strategy, broad portfolio and
successful commitment to industrial metaverse
- Siemens
manager Virginie Maillard elected to the Metaverse Standards Forum’s board of
directors
Siemens is
the leading international provider in the growing industrial metaverse market,
according to the latest PAC RADAR from PAC, the renowned market research
company specializing in business software, IT services and digital
transformation. This rating is based on three aspects: a clear strategy, an
existing portfolio and the progress Siemens is making in this area.
- Number of people in the company’s educational programs in Germany grows 15 percent: more than 1,500 apprentices and participants in work-study programs to start their careers at Siemens in 2023
- Almost all apprenticeships and work-study positions on offer focus on jobs in technical areas, including IT
- Siemens and FAU are cooperating for a new English-language master’s program in sustainability management
More than 1,500 apprentices and participants in work-study programs in Germany will start their careers at Siemens on September 1. Despite the scarcity of applicants in the country’s apprenticeship market, this number has significantly increased compared to the previous year (2022: 1,300; 15 percent increase). For a while now, there has been an imbalance between supply and demand on Germany’s apprenticeship market: At the start of August, more than 220,000 training positions were reported as vacant. However, only around 117,000 of the country’s young people are currently looking for an apprenticeship.
- Heliox expands Siemens eMobility’s offering for the growing eBus and eTruck charging market, and for depot and fleet solutions
- Accelerates value creation in Siemens’ fast-growing eMobility business
- Adds attractive digitalization and software potential
Siemens AG
has signed an agreement to acquire Heliox, a Netherlands-based technology
leader in fast charging solutions, serving e-Bus and e-Truck fleets and
passenger vehicles. The acquisition will complement Siemens’ existing eMobility
charging portfolio, adding products and solutions for DC fastcharging focused
on eBus and eTruck fleets. Heliox’s portfolio will also extend Siemens’ market reach,
primarily in Europe and North America, while improving capabilities in power electronics.
The transaction is subject to customary regulatory approval.
We released our third quarter results for fiscal year 2023 on August 10, 2023. The Press Conference Call and the Analyst Call were broadcast live.
- Orders rose 15 percent on a comparable basis to €24.2 billion and again reached a very high level (Q3 2022: €22.0 billion)
- Revenue grew 10 percent on a comparable basis to €18.9 billion (Q3 2022: €17.9 billion)
- Profit Industrial Business totaled €2.8 billion (Q3 2022: €2.9 billion) with a strong increase at Smart Infrastructure and Digital Industries
- Net income was €1.4 billion (Q3 2022: a net loss of €1.5 billion)
- Free cash flow all-in at group level was an outstanding €3.0 billion, a 29 percent increase (Q3 2022: €2.3 billion)
- Outlook on group level confirmed for fiscal 2023 for revenue growth and EPS pre PPA, excluding the Siemens Energy Investment
Siemens continued
its profitable growth trajectory in Q3 2023 (ended June 30, 2023),
with all industrial businesses achieving strong revenue growth. Order momentum
in the company’s major projects and systems business was also strong. The
book-to-bill ratio was an excellent 1.28, while the order backlog of €110 billion
was again at a record high level. Siemens confirms its outlook on group level
for fiscal 2023 and continues to expect revenue growth of 9 percent to 11 percent
and basic earnings per share before purchase price allocation accounting (EPS
pre PPA) of €9.60 to €9.90, excluding the Siemens Energy Investment.
- Monitoring of all 3-phase grids from 200 V to 690 V nominal voltage
- Frequency monitoring from 15-70 Hz for more detailed information
- IO-Link enables transmission and evaluation of measured values in the
controller or higher-level systems
- Certification according to SIL 1 (IEC 62061) and PL c (EN ISO 13849-1)
standards for a wide range of applications
Siemens has launched a new generation of line monitoring relays. The SIRIUS 3UG5 line monitoring relays combine proven technology with new functions and applications. The relays are the easiest way to monitor standards-compliant grid stability and quality, ensuring proper system operation and a long service life of components such as motors or compressors. Grid monitoring relays are used in critical areas such as hospitals or the process industry, which require a high-quality, fail-safe supply of power. Other areas of application include cranes, elevators, air, and air-conditioning compressors, as well as the timber industry.
- Siemens to donate EUR 500,000 to foundation for mountain rescue services
- Funds to further develop globally unique Bavarian Mountain Rescue Service's center for Safety and Training in Bad Tölz
- Half of donations from Siemens employees
Siemens and
the charitable association Siemens Caring Hands e.V. are supporting the Stiftung
Bergwacht, a non-profit foundation for mountain rescue services, with a
donation of €500,000. The foundation will use the donation to further develop
the Bavarian Mountain Rescue Service’s Center for Safety and Training in Bad
Tölz, Germany, and thus improve disaster prevention in Germany and Europe. Half
the donation is from Siemens employees and half from Siemens AG. The funds are part
of a donation pool that Siemens set up in 2021 in response to the flood
disaster on the Ahr River in the German states of Rhineland-Palatinate, North
Rhine-Westphalia and Bavaria. Over the past two years, €2.8 million from the
pool has been used to support 25 emergency, reconstruction and prevention
projects.
- Innovative Sentron 3WA circuit breaker series part of Siemens Xcelerator
- Designed to improve ease of use, reliability, and digitalization when integrating into existing systems
- Essential for critical infrastructure, such as hospitals or data centers
- 3WA1 (IEC), 3WA2 (UL489), and 3WA3 (UL1066+IEC) offer worldwide compatibility
Siemens has launched two new additional
versions of its innovative Sentron 3WA Power Circuit Breakers, alternatively
known as Air Circuit Breakers (ACBs). Series 3WA3 meets the requirements of UL
1066 and IEC 60947-2 standards, which enables customers to use it worldwide.
This is particularly advantageous for switchgear manufacturers and OEMs producing
systems for both standardization areas – IEC and UL. The 3WA2 series is
designed exclusively for the UL 489 market. The two new ACB model series
complement the 3WA1 version for IEC markets, which has been launched in the
fall of 2020. Siemens offers a full range of ACBs which are based on a
consistent system and offer great flexibility for applications around the
globe. The Sentron 3WA Power Circuit Breakers are part of the Siemens
Xcelerator portfolio. Siemens Xcelerator is an open digital business platform
that enables customers to accelerate their digital transformation easier,
faster, and at scale.
Siemens is rigorously executing its announced €2 billion investment strategy. Of this amount, the company plans to invest around €1 billion in Germany, thereby boosting the country’s innovative strength.