- Siemens smart buildings portfolio, including Building X, recognized as Accredited Solutions by WiredScore
- WiredScore sets a global standard for technology in the built world
- SmartScore certification by WiredScore supports global investors and building operators to implement smart, connected buildings according to highest industry benchmarks and tenant expectations
- Accreditation underlines Siemens’ commitment to support customers in achieving smart and future-poof buildings
Siemens Smart Infrastructure’s smart buildings portfolio, designed to help building
owners create healthy, comfortable, and sustainable buildings – whether greenfield
or retrofits – has been recognized by WiredScore’s Accredited Solutions. The
accreditation for smart solution providers is granted by WiredScore, a US-based
company that sets a global standard for technology in the built world through
certification and education.
- Investment of CHF250 million creates climate neutral campus for 1,700 colleagues
- State-of-the-art sustainability flagship built by combining real and digital worlds
- Inauguration of R&D facility marks final addition to the Siemens Campus in Zug
- Siemens Smart Infrastructure business aims to advance technology for a greener future
Siemens
today inaugurated a new Research and Development (R&D) facility in the
presence of Swiss Economy Minister Guy Parmelin, Canton Zug Government
Councilor Silvia Thalmann-Gut and Roland Busch, the President and CEO of
Siemens AG, to mark the completion of its CHF250 million investment and the
seven-year construction of its climate-neutral campus in Zug, Switzerland.
- Northumbrian Water Group to connect more than one million smart water meters to Siemens data management system
- Cloud-based system will identify household leaks to help reduce water consumption and support Ofwat targets
- Siemens solution represents the company’s largest ever deployment of grid software
- EnergyIP® MDM X for Water software is part of the Siemens Xcelerator portfolio
Siemens Grid Software has secured a new contract with Northumbrian Water Group and deployed EnergyIP® MDM X, part of the Siemens Xcelerator portfolio. Northumbrian Water Group (NWG) is enhancing its ability to detect and reduce household water leaks by connecting more than one million smart water meters to a new Siemens data management platform by 2030.
- Monitoring of all 3-phase grids from 200 V to 690 V nominal voltage
- Frequency monitoring from 15-70 Hz for more detailed information
- IO-Link enables transmission and evaluation of measured values in the
controller or higher-level systems
- Certification according to SIL 1 (IEC 62061) and PL c (EN ISO 13849-1)
standards for a wide range of applications
Siemens has launched a new generation of line monitoring relays. The SIRIUS 3UG5 line monitoring relays combine proven technology with new functions and applications. The relays are the easiest way to monitor standards-compliant grid stability and quality, ensuring proper system operation and a long service life of components such as motors or compressors. Grid monitoring relays are used in critical areas such as hospitals or the process industry, which require a high-quality, fail-safe supply of power. Other areas of application include cranes, elevators, air, and air-conditioning compressors, as well as the timber industry.
- Innovative Sentron 3WA circuit breaker series part of Siemens Xcelerator
- Designed to improve ease of use, reliability, and digitalization when integrating into existing systems
- Essential for critical infrastructure, such as hospitals or data centers
- 3WA1 (IEC), 3WA2 (UL489), and 3WA3 (UL1066+IEC) offer worldwide compatibility
Siemens has launched two new additional
versions of its innovative Sentron 3WA Power Circuit Breakers, alternatively
known as Air Circuit Breakers (ACBs). Series 3WA3 meets the requirements of UL
1066 and IEC 60947-2 standards, which enables customers to use it worldwide.
This is particularly advantageous for switchgear manufacturers and OEMs producing
systems for both standardization areas – IEC and UL. The 3WA2 series is
designed exclusively for the UL 489 market. The two new ACB model series
complement the 3WA1 version for IEC markets, which has been launched in the
fall of 2020. Siemens offers a full range of ACBs which are based on a
consistent system and offer great flexibility for applications around the
globe. The Sentron 3WA Power Circuit Breakers are part of the Siemens
Xcelerator portfolio. Siemens Xcelerator is an open digital business platform
that enables customers to accelerate their digital transformation easier,
faster, and at scale.
- Independent analyst firm has recognized Siemens Smart Infrastructure as a leader in integrated smart building security software
- The software is part of the Siemens Xcelerator portfolio
Industry analyst firm Verdantix has ranked Siemens Smart Infrastructure as one of the leading providers for security software in smart buildings. Their recently published “Green Quadrant: Integrated Smart Building Security Software 2023” report analyzes and evaluates ten companies that are shaping the market. Verdantix noted that Siemens solutions offer highly advanced unified security management capabilities. The assessed Siemens software is part of Siemens Xcelerator, an open digital platform that enables customers to accelerate their digital transformation.
- Innomotics, a leading supplier of
motor and large-drive systems, has launched with a new brand identity
- As of July 1, 2023, Innomotics has
become a separately managed Siemens subsidiary in Germany
- Global carveout is on track and is to
be largely completed by October 1, 2023
- Operating headquarters are in
Nuremberg, Germany, for the new company, which employs about 15,000 people
globally and generates more than €3 billion in revenue
Innomotics has
launched in Germany as a separately managed legal entity as of July 1,
2023. Under a single roof, the supplier of motors and large drives brings together
business activities with low- to high-voltage motors, geared motors,
medium-voltage converters and motor spindles as well as project and service
offerings for this product portfolio. The company’s operating headquarters are
located in Nuremberg, Germany. The carveout in Germany has now been completed. The
global carveout is also to be largely completed by the beginning of the new
fiscal year on October 1, 2023. In the future, Innomotics will comprise the previous
corresponding businesses from the units Large Drives Applications and Digital
Industries, as well as the separately managed Siemens companies Sykatec and
Weiss Spindeltechnologie. Worldwide, around 15,000 people are working at
Innomotics to realize growth potential and thus secure the company’s future market
success as a trailblazing specialist for motors and large drives.
- LV Insights X software key to accelerating energy transition and path to net zero
- Future-proof software to increase grid capacity in existing power networks
- Distribution grid operators can set up digital twin of low-voltage grids
- Reduced outage times by up to 30 percent, increased insights on critical segments, capacity and limit violations of power grid
- LV Insights X is part of the Siemens Xcelerator portfolio
Siemens is taking
another important step to accelerate the energy transition: As an industry
first, the company today presented its newly developed software for low-voltage
grids. LV Insights X software, part of the Siemens Xcelerator portfolio,
enables distribution grid operators (DSO) to tackle their most pressing
challenge: the need to significantly increase grid capacity while grids are
already pushed to their limits by the fast increase of decentralized renewable
energy infeed and additional consumers such as EV chargers or heat pumps. To avoid
power grids from becoming the bottleneck of the energy transition, utilities urgently
need to increase their grid capacity and actively manage the low-voltage grid.