- Northumbrian Water Group to connect more than one million smart water meters to Siemens data management system
- Cloud-based system will identify household leaks to help reduce water consumption and support Ofwat targets
- Siemens solution represents the company’s largest ever deployment of grid software
- EnergyIP® MDM X for Water software is part of the Siemens Xcelerator portfolio
Siemens Grid Software has secured a new contract with Northumbrian Water Group and deployed EnergyIP® MDM X, part of the Siemens Xcelerator portfolio. Northumbrian Water Group (NWG) is enhancing its ability to detect and reduce household water leaks by connecting more than one million smart water meters to a new Siemens data management platform by 2030.
- Monitoring of all 3-phase grids from 200 V to 690 V nominal voltage
- Frequency monitoring from 15-70 Hz for more detailed information
- IO-Link enables transmission and evaluation of measured values in the
controller or higher-level systems
- Certification according to SIL 1 (IEC 62061) and PL c (EN ISO 13849-1)
standards for a wide range of applications
Siemens has launched a new generation of line monitoring relays. The SIRIUS 3UG5 line monitoring relays combine proven technology with new functions and applications. The relays are the easiest way to monitor standards-compliant grid stability and quality, ensuring proper system operation and a long service life of components such as motors or compressors. Grid monitoring relays are used in critical areas such as hospitals or the process industry, which require a high-quality, fail-safe supply of power. Other areas of application include cranes, elevators, air, and air-conditioning compressors, as well as the timber industry.
- Innovative Sentron 3WA circuit breaker series part of Siemens Xcelerator
- Designed to improve ease of use, reliability, and digitalization when integrating into existing systems
- Essential for critical infrastructure, such as hospitals or data centers
- 3WA1 (IEC), 3WA2 (UL489), and 3WA3 (UL1066+IEC) offer worldwide compatibility
Siemens has launched two new additional
versions of its innovative Sentron 3WA Power Circuit Breakers, alternatively
known as Air Circuit Breakers (ACBs). Series 3WA3 meets the requirements of UL
1066 and IEC 60947-2 standards, which enables customers to use it worldwide.
This is particularly advantageous for switchgear manufacturers and OEMs producing
systems for both standardization areas – IEC and UL. The 3WA2 series is
designed exclusively for the UL 489 market. The two new ACB model series
complement the 3WA1 version for IEC markets, which has been launched in the
fall of 2020. Siemens offers a full range of ACBs which are based on a
consistent system and offer great flexibility for applications around the
globe. The Sentron 3WA Power Circuit Breakers are part of the Siemens
Xcelerator portfolio. Siemens Xcelerator is an open digital business platform
that enables customers to accelerate their digital transformation easier,
faster, and at scale.
- Independent analyst firm has recognized Siemens Smart Infrastructure as a leader in integrated smart building security software
- The software is part of the Siemens Xcelerator portfolio
Industry analyst firm Verdantix has ranked Siemens Smart Infrastructure as one of the leading providers for security software in smart buildings. Their recently published “Green Quadrant: Integrated Smart Building Security Software 2023” report analyzes and evaluates ten companies that are shaping the market. Verdantix noted that Siemens solutions offer highly advanced unified security management capabilities. The assessed Siemens software is part of Siemens Xcelerator, an open digital platform that enables customers to accelerate their digital transformation.
- LV Insights X software key to accelerating energy transition and path to net zero
- Future-proof software to increase grid capacity in existing power networks
- Distribution grid operators can set up digital twin of low-voltage grids
- Reduced outage times by up to 30 percent, increased insights on critical segments, capacity and limit violations of power grid
- LV Insights X is part of the Siemens Xcelerator portfolio
Siemens is taking
another important step to accelerate the energy transition: As an industry
first, the company today presented its newly developed software for low-voltage
grids. LV Insights X software, part of the Siemens Xcelerator portfolio,
enables distribution grid operators (DSO) to tackle their most pressing
challenge: the need to significantly increase grid capacity while grids are
already pushed to their limits by the fast increase of decentralized renewable
energy infeed and additional consumers such as EV chargers or heat pumps. To avoid
power grids from becoming the bottleneck of the energy transition, utilities urgently
need to increase their grid capacity and actively manage the low-voltage grid.
- Pfizer’s new high containment production plant is one of the world’s most modern and sustainable; uses 40% less energy for environmental control than traditional facilities
- Special containment concept, monitored and controlled by Building Services from the Siemens Xcelerator portfolio, boosts safety for employees handling high-potency ingredients
- Siemens technology integrates building and production data via Desigo CC
Pharmaceutical
company Pfizer has opened a new high-containment manufacturing facility in
Freiburg, Germany, using technology and services from Siemens to make it one of
the most modern and sustainable of its kind. Potentially producing up to seven
billion tablets a year for more than 180 countries, the plant uses an
innovative containment concept - monitored and controlled by Building Services
from Siemens Xcelerator portfolio - which ensures employee safety and results
in a 40 percent reduction in energy use in its environmental control system,
compared to a traditional facility.
- SICAM 8 delivers a universal automation platform for all applications in the field of power supply
- Incorporates SICAM HMI, elevating process visualization to the next level
- Includes the SICAM S8000 software solution for power automation
- SICAM 8 platform forms part of the Siemens Xcelerator portfolio
Siemens Smart
Infrastructure has launched the highly scalable SICAM 8 power automation
platform. Designed with scalability and security at its core, the platform helps
customers achieve resilient and secure grid operation, while allowing for the
incorporation of additional applications in the future. It also includes two
new software solutions: the SICAM HMI (Human Machine Interface) visualization
tool and the SICAM S8000 software solution for power automation, and forms part
of the Siemens Xcelerator portfolio, an open digital platform that enables
customers to accelerate their digital transformation easier, faster, and at
scale.
- Acquisition to strengthen Siemens’ capability to address fast-growing
demand for electric vehicle charging infrastructure in India, expand local
market presence, enable creation of export hub
- To scale up Siemens’ range of e-mobility solutions in India,
complementing its global portfolio
- Closing
subject to fulfilment of condition precedents as agreed between the parties and
receipt of requisite regulatory, statutory and other approvals
In a step to address the fast-growing demand for
electric vehicle (EV) charging infrastructure in India, Siemens Limited, signed
an agreement today to acquire the EV division of Mumbai-based Mass-Tech
Controls Private Limited. The division is engaged in design, engineering and
manufacturing of a wide range of AC chargers, and 30 to 300kW capacity DC
chargers for various end applications for EVs. The cost of the acquisition is
approximately Rs. 380 million (EUR 4.3 million) on a cash free and debt free
basis and subject to other adjustments that are mutually agreed between the
parties to the transaction.