- Siemens will supply three Dresser-Rand® 5HHE-VL-3NL reciprocating compressors for what will become the largest hydrogen production unit in the United States.
A leading industrial gas company recently selected Siemens to supply three Dresser-Rand® 5HHE-VL-NL reciprocating compressors for a new, state-of-the-art steam methane reformer (SMR) in Texas. The SMR will provide high-purity hydrogen for the gas company’s customers throughout the region.
- Siemens' broad energy portfolio and services will help ensure long-term reliability and efficient operations
- Integrated, redundant plant design features two SGT-600 gas turbines with DLE technology running on residue gas with high concentrations of hydrogen
- Project highlights the integrated value of Siemens Gas and Power
Braskem, the largest petrochemical company in Latin America, recently entered into an agreement with Siemens to modernize a cogeneration power and steam plant at its Petrochemical Complex in Sao Paulo, Brazil. Completion of the project is expected in early 2021.
- 1.3-gigawatt turnkey combined cycle power plant
- Long-term service program and operation & maintenance (O&M) services included
- Largest LNG-to-power development in Latin America
- Total project volume of €1 billion
Siemens has secured an order for the turnkey construction of a new combined cycle power plant for the integrated LNG-to-Power project GNA 1 of Gás Natural Açu in the Port of Açu in the state of Rio de Janeiro, Brazil. Siemens is providing an equity investment and owns one-third of the project company Gás Natural Açu (GNA) together with Brazil logistics company Prumo Logística S.A. and BP. In addition, Siemens signed a long-term service agreement and will operate and maintain the plant to help ensure reliability, availability and operational performance. The order is the first application for the highly efficient and proven Siemens H-class gas turbine in Brazil. With a capacity of approximately 1.3 gigawatts (GW), the power plant will provide affordable and clean energy for Brazil. Total project volume for GNA 1 is approximately €1 billion (R$4.5 billion).
- SensgearTM technology launch for digital connectivity of switchgear products
- New Sensformer® advanced with applications based on digital twin simulation of transformers
- Portfolio extension comes with comprehensive data analytics for added transparency, enhanced productivity, and advanced intelligence
Siemens is introducing Sensgear, its new digital switchgear portfolio, and the Sensformer advanced at this year's Hannover Messe. With the combination of the already well-established digitally connected transformer, the Sensformer, and the new Sensgear technology, all substation transmission assets are now fully connective, allowing operators to check their status via online applications in real time. Gas-insulated switchgear, circuit breakers, surge arresters, disconnectors, instrument transformers, and coil products will henceforth be equipped with Sensgear technology. All devices are connected via a smart and robust Internet of Things (IoT) gateway that securely transmits the required information to a cloud-based storage and visualization platform. All Sensgear products provide additional transparency with GPS and local weather information as well as product-specific measurement data that includes gas density, liquid temperature, gas leakage, and switching position.
- Services support first use of Siemens H-class turbine in an aluminum smelting facility globally
- Siemens' first long-term service agreement in the UAE for an H-class turbine
- Power services will ensure reliable operations for stable power production
Emirates Global Aluminum (EGA), the world's largest 'premium aluminum' producer, and Siemens announced the first power services agreement for an H-class gas turbine in the United Arab Emirates (UAE). With the new 20-year service agreement, Siemens will provide maintenance and repairs as well as onsite personnel support for the gas turbine and its generator at the planned over 600-megawatt (MW) combined cycle project feeding EGA's Jebel Ali power plant in Dubai.
- Real-time data analysis from 29 gas turbines across multiple locations will increase availability, reduce forced outages and enable proactive, prescriptive maintenance
- Digitalization to improve availability, efficiency, productivity and flexibility
Siemens will install state-of-the-art Remote Diagnostic Services (RDS) for GAIL (India) Limited covering 29 gas turbines operating across the Hazira-Vijaipur-Jagdishpur (HVJ) pipeline and the Vijaipur C2/C3 Plant. The scope includes the supply of RDS hardware, site installation and commissioning including remote Operational Service Desk (OSD) and helpdesk services. The OSD will be accessible 24/7, equipped with machine learning tools and manned by technical experts to provide faster, high quality troubleshooting and guidance for problem resolution.
- Designed to optimize customers' asset value and performance for coal and steam-based power plants
- Siemens experts will work alongside customers to co-create solutions that help deliver higher efficiency, reliability and flexibility in operations
Siemens experts will work alongside customers to co-create solutions that help deliver higher efficiency, reliability and flexibility in operationsSiemens has officially opened its new MindSphere Application Center in India. The facility is a state-of-the-art digitalized technology center, supported by Siemens’ MindSphere, an open, cloud-based IoT operating system that lets customers connect machines and physical infrastructure to the digital world and their thermodynamic digital twins.
Additive manufacturing has the potential to become a new key technology. For example it opens up new attractive prospects in the manufacture of gas turbines. This is why Siemens has been investing in this innovative technology right from its inception, and is now driving the industrialization and commercialization of these processes. Additive Manufacturing is a process that builds parts layer-by-layer from sliced CAD models to form solid objects. This enables highly precise solutions to be formed from powdered high-performance materials. Siemens is a pioneer in Additive Manufacturing and already uses the technology for rapid prototyping. Furthermore the company is now developing solutions ready for series-production for manufacturing gas turbine burner nozzles and repairing burner heads. Just recently Siemens achieved yet another breakthrough: the first gas turbine blades ever to be produced using Additive Manufacturing have successfully finished performance testing under full-load conditions.
- Siemens to supply 19 net-gas, off-gas and recycle gas compressors for crude flexibility project
- The project will enable the refinery to process up to 420,000 barrels per day of offshore crude oil
Siemens was recently selected to provide 19 process reciprocating compressors for ADNOC Refining’s crude flexibility project at Ruwais Refinery-West. The project is intended to increase the refinery’s crude processing flexibility, enabling the site to process up to 420,000 barrels of oil per day of the local crude grade known as Upper Zakum, which is found offshore. The upgrade will improve the value of each barrel of oil and allow ADNOC to export more of its main onshore, lighter-grade Murban crude.
Agility is the ability to adjust rapidly to changing market conditions, capitalize on emergent business opportunities, and reduce costs or increase revenue streams in the process. In the wake of decarbonization, decentralization, and digitalization, it is the basis for grid operators' and utilities' future business success.
The Siemens booth at EUW 2018 presented combined solutions for electrification, automation, and digitalization that pave the way for multilayered, distributed, and connected grids, this way enabling the required degree of agility.