- Siemens, MW Storage International, Fluence and Vibeco develop unique ecosystem for global beverage manufacturer
- Solution to enable new levels of energy optimization
- Encompasses software, financing, latest storage technology
- Sinebrychoff’s first energy storage service contract
In a move that brings new market opportunities for industrial players, Siemens has developed a unique business model to support the next level of energy optimization for Finnish brewery Sinebrychoff, a subsidiary of the international Carlsberg Group. At the heart of the solution, which will be implemented at Sinebrychoff’s plant in greater Helsinki, is a virtual power plant (VPP) and the latest energy storage technology, supported with financing solutions, to create one of the first examples of power flexibility in an industrial site.
- Siemens presents the first virtual additive manufacturing reference factory for selective laser sintering and industrial post-processing with its partners EOS and DyeMansion
- End-to-end software and automation solutions from the Digital Enterprise portfolio drive the industrialization for leading technology providers and users of additive manufacturing
Under the motto "Partnering for the next step to industrialize Additive Manufacturing", Siemens is going to present at Formnext Connect its Digital Enterprise Portfolio for the industrialization of additive manufacturing as well as innovations with partners around new achievements in various additive manufacturing technologies. One highlight is the partnership with EOS and DyeMansion. Together, the three companies will present the first virtual additive manufacturing reference factory for selective laser sintering with polymers. Using the example of a midsole for footwear applications in which parameters such as design, fit and color are individually and economically taken into account, Siemens, EOS and DyeMansion will demonstrate what the next step towards the industrialization of selective laser sintering with polymers can look like along the entire production chain. "The automated chain of coordinated production steps from all suppliers, from design and printing to post-processing, as well as end-to-end IT integration, is crucial for high productivity and maximum flexibility. This applies to series parts as well as to a highly flexible lot-size-1 production for individualized products or spare parts," explains Dr. Karsten Heuser, Vice President Additive Manufacturing at Siemens Digital Industries, and continues: "With the end-to-end digitization and automation solutions from Siemens, we have succeeded, together with our partners EOS and DyeMansion, in creating a seamlessly integrated end-to-end value chain for industrial additive manufacturing with selective laser sintering and industrial post-processing solutions using polymers.”
- Proven process optimization from basic level control to complex pumping routines
- Programmable features reduce maintenance and companies’ carbon footprints
- Wide range of applications in environmental and general industries
Siemens presents the new Sitrans LT500 level, flow, and pump controllers for radar and ultrasonic transmitters or any other two-wire 4-20 mA devices. From basic level control to complex pumping routines, these instruments deliver the accuracy and reliability demanded by a variety of applications. Complete with up to 2 measuring points, 6 control or alarm relays, 2 discrete inputs, 3 analog outputs, and communications options, Sitrans LT500 is an attractive option for your controller applications.
- Siemens industrializes additive manufacturing with polymers with EOS and DyeMansion as partners
- Siemens and EOS support Hexr in the mass customization of additively manufactured bicycle helmets
- Digital Enterprise portfolio offers integrated software and automation solutions for the industrialization of additive manufacturing
- Additive Manufacturing Network – an online order-to-delivery collaboration platform for the industrial additive manufacturing community, helps streamline the AM production process
Siemens' Digital Enterprise portfolio consists of software and automation solutions that optimize process steps along the entire value chain of additive manufacturing. This holistic approach is unique in the field of the industrialization of additive manufacturing. "The automated chain of coordinated production steps from all suppliers, from design and printing to post-processing, as well as end-to-end IT integration, is crucial for high productivity and maximum flexibility. This applies to series parts as well as to a highly flexible lot-size-1 production for individualized products or spare parts," explains Dr. Karsten Heuser, Vice President Additive Manufacturing at Siemens Digital Industries.
- Strategic partnership for digital transformation of pharmaceutical processes
- Operational usage of digital plant data
- New Smart Engineering Services (SES)
- New modules improve integration in the value chain
Siemens and Zeta have entered
into a strategic partnership. The aim of both companies is to drive forward the
digital transformation of pharmaceutical processes worldwide. Zeta, a
specialist with many years of experience in major projects for the
biopharmaceutical industry, takes the role of the system integrator thanks to
their process expertise from the pharmaceutical sector. In partnership with
Zeta, Siemens acts as the system provider offering software platforms with
their Digital Enterprise Portfolio. The Comos plant engineering software
solution is the basis for the digital engineering platform, with
object-oriented data management and the use of intelligent templates for the
implementation of pharma-specific planning processes. In addition to the
integration of existing platform functions, Zeta and Siemens are developing new
modules to further improve the integration of the value chain.
- Sinamics G115D comprises motor, frequency converter and gear box and is available as one complete solution in a motor-mounted and wall-mounted version
- Comprehensive TIA portal and Startdrive integration simplifies commissioning
- Compatibility with MindConnect portfolio enables cloud-based analysis
With
Sinamics G115D, Siemens presents a new, compact, and powerful drive system
specifically designed for horizontal conveyor applications. The drive system
comprises motor, frequency converter and gearbox in one unit and is offered in
two versions – wall-mounted and motor-mounted. The Sinamics G115D drive system
is characterized by a robust design with a high IP protection class (up to
IP66) and is therefore also suitable for use in harsh environments. Thanks to
its compact dimensions, the Sinamics G115D can be installed easily even in
confined areas. The drive system can also be operated reliably over a wide
temperature range of -30 to 55 degrees Celsius. The Sinamics G115D drive system
is suitable for applications in intralogistics and airports as well as in the
automotive and food & beverage industries and is available in the power
ranges 0.37 to 7.5 kilowatts for wall mounting and 0.37 to 4 kilowatts for
motor mounting. The drive system can be put into operation quickly and easily
with comprehensive integration into the TIA (Totally Integrated Automation)
portal including the Startdrive commissioning software, or the Sinamics G120 Smart
Access Module (SAM) web server tool for setup and diagnostics. To be prepared
for the digital transformation and to enable cloud-based analyses, Sinamics
G115D is integrated into the entire MindConnect portfolio and is compatible
with Mindsphere applications such as Analyze MyDrives.
- Siemens to offer industry’s first integrated multiscale solution for soft matter as part of Simcenter portfolio
- Addition of Culgi technology to enable performance-driven optimization of advanced materials in both discrete and process manufacturing industries
Siemens announced
today that it has signed an agreement to acquire Culgi, a computational
chemistry software company with a focus on multiscale simulations in the
process industries. Culgi will join Siemens Digital Industries Software, where
its solutions will expand simulation capabilities of the
Xcelerator
™
portfolio with quantum and molecular chemistry models that seamlessly couple
with the continuum approach in
Simcenter™ STAR-CCM+™ software. This unique engineering workflow can deliver
significant cost savings and accelerate innovation in the materials and process
industries, increasing the potential for product and process transformations.
- Siemens is the exclusive global sales partner for Moby.Check in the process industry
- Simple functional solution offers advantages for mobile servicing and maintenance procedures as well as for production and logistic operations in the process industry
- Audit-proof storage of testing and maintenance tasks
- Stand-alone solution can be integrated easily into existing maintenance or ERP systems
Siemens and Log.Go.Motion - a specialist in the digitalization of processes in industry and logistics - have concluded a cooperation agreement.Effective immediately, Siemens is the exclusive global third-party distributor for the Moby.Check software solution within the process industry. Moby.Check can be used to create, control, and monitor individual digital inspection checklists for servicing and maintenance procedures as well as for production and logistics processes. The software system has been developed for global use in industry.
- Robotic fiber placement and 3D printing enable disruptive breakthroughs in today’s manufacturing processes thanks to the advantages promised by Industry 4.0, the Digital Twin, higher robotic intelligence and complex motion control.
Siemens and Ingersoll Machine Tools have expanded their decade-long partnership to support the Rockford, IL-based machine tool company of Camozzi Group on its digital journey of creating digital twins of its products and expanding into new markets. Based upon extensive experience in heavy machine tool building, Siemens cutting-edge technologies in hardware complement Ingersoll Machine Tools’ successful journey into the new market of additive manufacturing and have pushed the boundaries for industrial robots for the aerospace market with its entry-level robotic platforms MasterPrint Robotic™ and MasterPrint Continuous Filament™.
- Sinumerik One Dynamics - three technology packages to increase the efficiency of CNC users when programming in the shopfloor and executing CAM-generated CNC programs
- Top Surface and Top Speed Plus for excellent motion control and perfect workpiece surfaces
With the software version NCU-SW 6.14, Siemens is launching three powerful technology packages exclusively for the CNC Sinumerik One. The Sinumerik One Dynamics packages are available in three different packages: One Dynamics Operate, One Dynamics 3-axis milling and One Dynamics 5-axis milling. The software functions contained in the technology packages support users from machine-oriented programming in the jobshop to high-performance machining of CAD-CAM-programmed workpieces with high surface quality.