- Contract awarded to Siemens for 2.2 megawatt PEM electrolysis plant
- Salzgitter Wind Hydrogen energy project gathers pace
- Goal is to achieve low-CO2 steelmaking based on Salzgitter’s innovative SALCOS technology concept
Salzgitter Flachstahl GmbH (SZFG) has awarded the contract to build a 2.2 megawatt PEM electrolysis plant (PEM = Proton Exchange Membrane) to Siemens Gas and Power, marking an important step towards hydrogen-based steelmaking. The plant is due to commence operation in the 4th quarter of 2020 and cover SZFG’s entire current demand for hydrogen. The necessary electrical power will be generated by seven wind turbines with a capacity of 30 megawatt. These will be erected by Avacon AG on the Salzgitter Group site and will likewise enter service from 2020.
- VAG Nürnberg orders 12 Avenio trams
- Option for up to 75 additional trams
- Innovative interior concept for enhanced passenger comfort
VAG
Verkehrs-Aktiengesellschaft Nürnberg has ordered 12 four-section Avenio trams.
The contract includes options for a total of up to 75 additional trams. The
trams will serve on possible new lines or be used to expand VAG’s existing offering.
Commissioning is planned for the end of 2022.
- Gas turbine rotor exchange allows for increased output and efficiency
- Control system upgraded to latest version of SPPA-T3000
The Dunamenti Power Plant in Százhalombatta, Hungary, is the largest gas-fired power plant in the country with a capacity of 794 megawatts (MW), making it a major source of reliable electricity in Hungary. Recently, in collaboration with the customer and plant owner, MET Asset Management AG, and within the scope of an overhaul project, Siemens Gas and Power replaced the entire rotor of the plant's SGT5-2000E gas turbine and installed a new, state-of-the-art SPPA-T3000 control system.
- Third Mireo order from DB Regio
- Service in the Karlsruhe 7b network
- Passenger comfort and sustainably increased value over entire lifecycle
DB Regio, the regional transport business of Deutsche Bahn AG, has
ordered seven Mireo trains from Siemens Mobility. The trains will operate on
the regional express route between Karlsruhe and Heidelberg/Mannheim via
Bruchsal in the Karlsruhe 7b network. They will be built at the Siemens
Mobility plant in Krefeld, Germany, and their delivery is planned for the end
of 2022.
- Two new indoor GIS systems increase power and ensure reliable supply
for consumers
- Clean Air products ensure
much more climate-friendly operation
- Turnkey solution provides
key support for transition to a new energy mix
German transmission grid operator TransnetBW
has commissioned Siemens to build new switchgear in the 380 kilovolt (kV)
Daxlanden substation in Karlsruhe, Baden-Württemberg. Two new gas-insulated
indoor switchgear, initially with 26 panels, will boost the substation's
transmission capacity and cover the increased transport demand in the German
high-voltage grid as a result of the transition to a new energy mix. In the
future, it will thus be possible to transport large quantities of wind energy
from northern Germany to the southern part of the country. Replacing sulfur
hexafluoride (SF6) with treated air, so-called Clean Air, as the insulating
medium in the bus ducts simultaneously ensures much more climate-friendly
operation. The commissioning of the turnkey solution will take place in stages
and be completed in 2029. The order is priced in the low triple-digit millions
range.
- Electrical capacity increased to approximately 1,200 megawatts
- Fired with regasified liquefied natural gas instead of oil
- Fifty percent lower CO2 emissions per kilowatt hour produced
Siemens will provide the equipment to upgrade the Hiep Phuoc 1 steam power plant in Ho Chi Minh City, Vietnam, to a combined cycle power plant. This project will increase the plant’s electrical capacity by roughly 780 megawatts (MW) to approximately 1,200 MW. The modernized plant will be fired with regasified liquefied natural gas (LNG) instead of the oil that has been used to date. By changing the fuel, deploying modern F-class gas turbines from Siemens, and using the waste heat from the gas turbines to produce electricity, the CO2 emissions can be cut almost in half for each kilowatt hour produced on-site. With this project, the customer Hiep Phuoc Power Co. Ltd., will ensure a reliable, secure, and environmentally friendly power supply for Ho Chi Minh City and Vietnam.
- First order from Asia for HL-class gas turbine
- New power plant with a capacity of more than one gigawatt
- Efficiency rating of more than 63 percent
Siemens will set up a high-efficiency HL-class power island for a new combined cycle power plant (CCPP) in South Korea. This will be the first two state-of-the-art HL-class gas turbines that Siemens will supply to a customer in Asia. The new plant, which will be built in Yeoju, in South Korea’s Gyeonggi Province, will run on regasified liquefied natural gas (LNG) and offer a generating capacity of more than one gigawatt. With a maximum efficiency rating of more than 63 percent the gas turbine will allow the power station to get the most out of the valuable LNG for electricity generation, enabling especially economical and environmentally friendly operation. The customer is South Korean EPC SK Engineering & Construction Co., Ltd., which is constructing the entire plant for the independent power producer Yeoju Energy Services.
- Campus Nyland test, training and signaling simulation center opens
- European Rail Traffic Management System (ERTMS) latest in intelligent infrastructure
- Nordlandsbanen will open first digital signaling railway in October 2022
Bane NOR and Siemens Mobility celebrated the opening of Campus Nyland, a test, training and signaling simulation center which will help the rail network operator prepare for the digitalization of the entire system. Norway has committed to becoming the first country to operate with a single digital interlocking and ERTMS signifies one of the country’s largest digitalization projects. In 2022, the first digital line, Nordlandsbanen, will open. In advance, the Campus Nyland center will prepare workers for working within the digital system, ERTMS. The intelligent infrastructure behind ERTMS will reduce operating costs and increase capacity throughout the network. In addition, it will enhance safety, with real-time visibility of trains across the network. When complete in 2034, the system will include 4,200 km of track and more than 350 stations.
- Key section of the Blue Line extension enters revenue service
- Features 14 new metro trains
- Greater availability and enhanced passenger experience
- Turnkey project includes metro trains, rail infrastructure, system integration, project management as well as service and maintenance
Mass Rapid Transit Authority of Thailand (MRTA) Bangkok Expressway and Metro Public Company Limited (BEM) and CH. Karnchang Public Company Limited launched revenue service on a key section of the Blue Line Extension in late September. BEM is operating 14 new metro cars delivered by Siemens Mobility on the extension. This is the latest milestone of the turnkey project which include delivering 35 three-car metro trains, the signaling system, the traction power supply, passenger information system, SCADA, depot workshop equipment, system integration and project management as well as a 10-year maintenance contract for the line’s expansion project. The full Blue Line extension will be commissioned in spring 2020.
A key milestone on the way to independence: Siemens Energy presented its new management team to its employees today. In addition to an Executive Board, the company will have an expanded international management team, the Group Management Committee. Once Siemens Energy becomes a legally separate entity, this team will be instrumental in implementing the company’s strategic approach. “Announcing the management team is a further critical step on the way to becoming an independent company and an energy pure play. It will enable Siemens Energy to further develop its management system and then focus fully on the requirements of its customers and markets,” said Joe Kaeser, President and CEO of Siemens AG.