- Modularized, high-pressure LNGo system helps bridge gap between remote gas supply and remote gas demand via "virtual pipeline"
- Altagas producing approximately 30,000 gallons of LNG per day, with capability to expand
Siemens' Dresser-Rand business recently commissioned an LNGo-HP (high-pressure) micro-scale natural gas liquefaction system for Altagas Ltd. in Dawson Creek, British Columbia, Canada. The modular, expandable LNGo technology enables efficient installation, especially in a demanding environment like Dawson Creek. The Dawson Creek facility, with a capacity of approximately 30,000 gallons of LNG per day, commenced production on January 25, 2018.
Highlighting its commitment to supporting Pakistan in meeting its growing power needs, Siemens has announced the signing of a long-term service agreement with Punjab Thermal Power (Private) Limited to provide comprehensive maintenance, parts and repair services for Punjab Power Plant Jhang for the next 12 years. The agreement includes Siemens' Power Diagnostics, part of the company's "Digital Services for Energy" portfolio of data-driven solutions.With the fifth-largest population in the world, Pakistan is working to spur socio-economic development by delivering reliable and efficient power supply to industries and homes. Located in Haveli Bahadur Shah, Punjab Power Plant Jhang, is expected to add 1.3 gigawatts (GW) to Pakistan's grid, making it one of the largest gas-fired, combined cycle power plants in the country. It will also see the first deployment of Siemens' SGT5-8000H gas turbines in the country, selected for their high power output and record-breaking efficiency. Anticipated benefits of the agreement include increasing the availability of the power plant and reducing the maintenance costs. The agreement covers all the scheduled and un-scheduled outage services for two SGT5-8000H gas turbines, generators, related auxiliaries as well as the supply of spare parts and field services."Pakistan's energy sector is undergoing a transformational period to meet the increasing demand of electricity. We are very proud to contribute to this significant project," said Gianluigi Di Giovanni, Senior Executive Vice President of Siemens Power Generation Services in the Middle East. "With our services, cross-fleet experience and digital capabilities, we look forward to bringing value and on-ground support to Punjab Thermal Power, helping maximize the potential of the plant's overall operations."Siemens' Power Diagnostics use advanced data analytics to help predict and eliminate unplanned downtime, and improve power plant productivity by identifying operational challenges in advance. It will also allow the power plant's team to manage outages more efficiently.The current agreement builds on Siemens' contributions towards strengthening Pakistan's power sector. It comes three months after the company signed the largest ever power generation contract in the country to provide a complete power island solution for Punjab Power Plant Jhang.
Building on its commitment to supporting the energy infrastructure in Sudan, Siemens has signed a long-term agreement with the Sudanese Thermal Power Generating Company (STPGC) to provide service and maintenance for the power generating assets and related components operating at the 337 megawatt (MW) Port Sudan and 502 MW Garri power plants.
- Exclusive equipment provider at each site which includes a long-term service agreement
- Project part of energy reform program to stimulate Mexico's economic growth
Siemens recently delivered five gas turbine-driven compressor trains to Fermaca Enterprises (Fermaca) for two pipeline stations in Mexico. The pipeline projects, which also include a long-term service agreement, are part of the Comision Federal de Electricidad de Mexico's (CFE) ongoing energy reform program intended to increase the availability of low-cost energy and stimulate the country's economic growth.
- Aeroderivative gas turbine will drive RFBB36 pipeline compressor
- Siemens compressor train for Winchell Lake Compressor Station for additional pipeline capacity
Siemens received an order from North American pipeline operator, Nova Gas Transmission Ltd. (NGTL), a wholly owned subsidiary of TransCanada Corporation, to supply a gas turbine-driven compressor train for the Winchell Lake Compressor Station in Alberta, Canada. The turbo-compressor train will be a critical part of the NGTL pipeline expansion to transport natural gas to export markets. Commercial operation is expected to begin in the fourth quarter of 2019.
On January 24, 2018, the most powerful high-voltage direct-current (HVDC) transformer began its journey from the transformer factory in Nuremberg, Germany, to China. The transformer will first be transported to the harbor in Nuremberg by special heavy load transporter, where it will be loaded onto a ship. Its journey will take it to Rotterdam via the Main-Danube Canal, and from there it will be shipped to China, where it will arrive after several weeks on the high seas. In July 2016, Siemens received an order to manufacture four transformers of this type. About a year later, the world’s first 1,100 kV transformer was completed and successfully passed the tests in the testing facility. The enormous dimensions of the transformer – 37.5 meters long, 14.4 meters tall, and 12 meters wide – posed a logistical challenge for the team. In operation, the transformer weighs just under 900 tons and its efficiency is well above 99% of the rated power. For the first time, the transformer will enable a high-voltage direct-current (HVDC) transmission with low losses over a record distance of 3,284 kilometers with a transmission capacity of 12 gigawatts. HVDC transformers are part of the converter station that convert alternating current into direct current at the beginning of the transmission line and convert it back again at the end of the line. The conversion from alternating current to direct current helps to transmit energy over long distances with low losses. Transformers are key components of an HVDC line: Thanks to the transformer, the Changji-Guquan project will be able to transmit direct current with a huge 1,110 kilovolts for the first time in the world. The new transformer not only makes the transmission of this record voltage level possible, but it is also the world’s most powerful tested transformer with a capacity of 587 megavoltamperes. Siemens has thus achieved a new dimension in high-voltage direct-current transmission. The HVDC line between Changji and Guquan will be operated by State Grid Corporation (SGCC), a Chinese grid operator. The connection is expected to begin operation in 2019.