- Designed for future power networks and digital substations
- Enhanced cyber security and communications
- User-friendly interfaces and software
With the new Reyrolle 5 series of protection relays, Siemens is further developing its offerings for medium-voltage and industrial power networks. The protection, control, monitoring and measuring of power networks is a vital element in managing electrical assets, increasing reliability, sustainability and the safety of operating personnel. The first device applications of the new generation of protection relay will be overcurrent and earth fault protection and transformer protection in substations. It includes comprehensive functionality as standard, with enhanced process data such as faults, events and waveform records enabling the power network to be effectively managed. The small number of device variants allows easy ordering and efficient engineering while the improved hardware platform makes it even easier to operate and manage the protection relays.
At this year’s European Utility Week (EUW) in Paris, Siemens Smart Infrastructure will demonstrate how it is driving energy intelligence across supply and demand. By helping shape the energy ecosystem across buildings, industry and the grid, Siemens is supporting government, cities and businesses with their sustainability goals. The company will focus on four topics that support the energy transition: sustainable grids, smart distribution, the Internet of Energy and grid edge.
By 2035, more than 50 percent of electricity is expected to be generated by renewables. In parallel, electricity consumption is forecast to double by 2050. Megatrends such as increasing urbanization and climate change are driving the need for electrification and decarbonization. Meanwhile, new applications in software and digitalization are making grids smarter and more efficient, creating new business models.
- New Grid Diagnostic Suite offers unique comprehensive insights
- Gain a grid-wide view of energy automation systems
- Market launch of initially four cloud-enabled applications
- Enhances cost efficiency and availability of smart grids
- Support through digitalization in increasingly complex power grids
Siemens is presenting for the first time its new Grid Diagnostic Suite at the European Utility Week in Paris. The Grid Diagnostic Suite initially includes four cloud-based applications which collect data from new or existing field devices for protection, distribution automation and power quality. These data are stored and analyzed in the cloud. This requires almost no additional engineering effort. Distribution grid operators and operators of electricity grids in industrial parks can quickly tap into useful information from devices installed anywhere in the smart grid. This will enable grid faults, for example, to be detected at an early stage and quickly rectified. After information is collected, vulnerabilities can be identified, and necessary measures can be implemented before any damage occurs. In this way, Internet of Things (IoT) applications in the Grid Diagnostic Suite enhance the availability of power grids while enabling them to be operated cost-efficiently.
- Highly compact design, up to 110 kiloamps
- Maintenance-free up to 10,000 interrupting cycles at current of 15 kA
- Based on proven HB3 generator platform with vacuum switching tech
Siemens is expanding its HB3 generator circuit-breaker portfolio with a new compact version. The HB3-Compact (HB3-C) offers the possibility for vertical or horizontal mounting and uses maintenance-free vacuum switching technology. These features make it especially valuable for retrofit applications in power plants, where the highest security of supply is crucial, and space is limited due to existing installations. The new system will be presented for the first time at the European Utility Week 2019, taking place in Paris from November 12 to 14.
- First soft starter series with integrated Safe Torque Off function
- Enhanced protection when shutting down electric motors
- High functional density saves space and decreases cost
Siemens Smart Infrastructure expanded its soft starters portfolio for motors, with the launch of Sirius 3RW55 Failsafe and Sirius 3RW50. Soft starters ensure electrical motors used in industry and infrastructure are protected during startup and ramp-down. The Sirius 3RW55 Failsafe soft starters are the first to feature the integrated Safe Torque Off (STO) function. As specified in safety standards, the protection function for electrical drive systems ensures that torque-generating energy stops acting when motors are turned off, preventing an unwanted restart. Control panel manufacturers no longer require using separate individual components to have this function, which reduces the time and effort for wiring and maintenance works and saves space in the control cabinet. In addition, the switching time of the integrated solution is significantly shorter than for conventional, electromechanical components.
- New Simotics HV M slipring motors provide range of power up to 4.5 MW
- Easy integration into SIDRIVE IQ applications for highest availability, serviceability, productivity and efficiency
- Easy plant integration due to 3-D Motor models to speed up complete plant integration processes
- Certified and proven Siemens MICALASTIC® VPI insulation system with extreme long lifetime
Building on more than a century of experience in manufacturing slipring motors, Siemens today announces the new Simotics HV M slipring motor. Designed and engineered for applications mainly in the cement and mining industries, the newest slipring motor is implemented in a wide range of applications including but not limited to mills, crushers, conveyors and fans. The new platform motor with its power range up to 4.5 MW completes the Siemens slipring motor family which covers now the power range from 0.5 to 8.2 MW.
Bane NOR, the state-owned agency responsible for the Norwegian national railway infrastructure, has contracted Siemens to upgrade the signaling equipment of the entire Norwegian rail network to the European Train Control System (ETCS). Commissioning of the rollout lines is scheduled to be completed by 2034. The contract also includes services for 25 years and is worth around 800 million euros in total.
At this year’s European Utility Week (EUW) in Paris, Siemens Smart Infrastructure will demonstrate how it is driving energy intelligence across supply and demand. By helping shape the energy ecosystem across buildings, industry and the grid, Siemens is supporting government, cities and businesses with their sustainability goals. The company will focus on four topics that support the energy transition: sustainable grids, smart distribution, the Internet of Energy and grid edge.
- Campus Nyland test, training and signaling simulation center opens
- European Rail Traffic Management System (ERTMS) latest in intelligent infrastructure
- Nordlandsbanen will open first digital signaling railway in October 2022
Bane NOR and Siemens Mobility celebrated the opening of Campus Nyland, a test, training and signaling simulation center which will help the rail network operator prepare for the digitalization of the entire system. Norway has committed to becoming the first country to operate with a single digital interlocking and ERTMS signifies one of the country’s largest digitalization projects. In 2022, the first digital line, Nordlandsbanen, will open. In advance, the Campus Nyland center will prepare workers for working within the digital system, ERTMS. The intelligent infrastructure behind ERTMS will reduce operating costs and increase capacity throughout the network. In addition, it will enhance safety, with real-time visibility of trains across the network. When complete in 2034, the system will include 4,200 km of track and more than 350 stations.
- Key section of the Blue Line extension enters revenue service
- Features 14 new metro trains
- Greater availability and enhanced passenger experience
- Turnkey project includes metro trains, rail infrastructure, system integration, project management as well as service and maintenance
Mass Rapid Transit Authority of Thailand (MRTA) Bangkok Expressway and Metro Public Company Limited (BEM) and CH. Karnchang Public Company Limited launched revenue service on a key section of the Blue Line Extension in late September. BEM is operating 14 new metro cars delivered by Siemens Mobility on the extension. This is the latest milestone of the turnkey project which include delivering 35 three-car metro trains, the signaling system, the traction power supply, passenger information system, SCADA, depot workshop equipment, system integration and project management as well as a 10-year maintenance contract for the line’s expansion project. The full Blue Line extension will be commissioned in spring 2020.