- ÖBB and Siemens Mobility show first painted car body
- New Nightjet trainsets enter service in 2022
- ÖBB aiming at greater passenger comfort and privacy
ÖBB and Siemens Mobility presented the first painted car body and exterior design for the new generation of the Nightjet in Vienna today. The new, ultra-modern trains will enter service near the end of 2022 and will first be used on connections from Austria and Germany to Italy. The first 13 trainsets have already been called up by ÖBB from a framework agreement with Siemens Mobility, and a further 20 trains are expected to be called up this year.
- One environment for planning, booking and settlement of multimodal travel
- Travel efficiently, comfortably, and sustainably
- Open ecosystem for all mobility providers
Siemens Mobility will sign a contract in the Netherlands with the joint venture RiVier (NS, HTM and RET) to develop a countrywide, intelligent Mobility as a Service (MaaS) platform. The MaaS platform to be delivered in the autumn will allow providers to integrate travel planning. The technological core of the MaaS platform is supplied by Siemens Mobility subsidiaries Hacon and eos.uptrade.
- Bus depot to be equipped with charging and power distribution technology
- 23 charging stations supply eBuses with 150 kW each
- Easy installation of power distribution system in the existing building thanks to busbar trunking technology
Siemens Smart Infrastructure has received an order from the Regensburg transport authority “das Stadtwerk Regensburg.Mobilität GmbH” in Germany to equip the bus depot in the Markomannenstrasse for electromobility. Siemens will supply the charging infrastructure as well as the power distribution technology. Operations are scheduled to start in 2021. Electric buses were first introduced in the city center of Regensburg in 2017.
Polish
provider of transport and logistics services Laude Smart Intermodal S.A. has
just expanded its fleet with the most modern locomotive in Europe: the Vectron
MS. The vehicle colored in pink was handed over in Poznan Franowo near Posen on
February 3
rd, 2021. It is the 50
th Vectron locomotive
from Siemens Mobility in the hands of Polish carriers.
- More flexibility thanks to KNX communication capability
- Less wiring reduces cost and saves inputs/outputs on the controller
- Ideal for noise sensitive applications thanks to <28 dB noise level
Siemens Smart Infrastructure has upgraded its range of SSA
actuators for small valves by adding new features for more energy efficient and
versatile hydronic room applications. The updated SSA actuators now offer more
flexibility due to their broad control possibilities - from analog control to
KNX communication capabilities for room solutions and fast integration into
connected systems. While using the same cable for communication and power, the
customer saves time and cost. Thanks to the operating mode ‘nightmode’, the
actuators are more silent than ever, with less than 28 dB. This makes them
ideal for use in noise-sensitive areas, such as hotels, recording studios,
meeting rooms and libraries.
- Order for double-decker Desiro HC trains and single-decker Mireo trains
DB Regio Bayern has ordered 31 regional trains from Siemens Mobility. The trains will serve on routes between Munich, Passau and Regensburg. Siemens Mobility will be delivering 25 double-decker Desiro HC trainsets and six single-decker Mireo trainsets. Passenger service with the new trains is planned to begin with the timetable change in December 2024.
-
- Cerberus PACE covers all PA/VA needs, from small and simple to large and complex applications
- Pro-quality sound with low latency
- Cost-efficient solution with no single point of failure
Siemens Smart Infrastructure has launched a new compact version of its CerberusPACE Modular system, further extending the range of applications in which the public address voice alarm (PA/VA) solution can be employed. Together, CerberusPACE Modular and Compact offer a comprehensive PA/VA solution, which can beintegrated with fire protection and danger management systems. This enables evengreater customization to protect lives, assets and business continuity.
- Aral to install more than 100 ultra-fast chargers at 30 gas stations in Germany until end of first quarter 2021; further roll-out planned
- Siemens to provide intelligent grid connection for growing power demand
- Cloud connection creates transparency across all locations, increases efficiency and reliability
Aral AG, a subsidiary of the bp group in Germany, has tasked Siemens Smart Infrastructure with expanding the grid connection at 30 selected gas stations. The installation of intelligent substations allows Aral to upgrade its gas stations with ultra-fast charging technology for electric vehicles. The installation is expected to be completed by the end of February.
- Voltage
range up to 1,000 V and scalable charging power up to 300 kW
- High
efficiency for reduced operational cost at high power flow
- Automated allocation and shifting of charging power
Siemens
Smart Infrastructure released its new public fast charger Sicharge D for the IEC markets. It is suited
for highway and urban fast charging stations, city parking as well as shopping
malls and provides one of highest peak efficiencies on the market at 96 percent,
scalable charging power and dynamic power sharing.