Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release07 June 2024Siemens MobilityErfurt
Franconia-Thuringia Express sprints with Siemens trains on the Nuremberg-Erfurt high-speed line
Bavaria’s Transport Minister
Christian
Bernreiter and
Heiko Büttner, DB Group Representative in Bavaria, together
with
Karl Blaim, Managing
Director and Chief Financial Officer of Siemens Mobility, officially inaugurated the fast
Regio train today at the futuristic railway station in Coburg and send it off
on its first trip to the Thuringian capital. In Erfurt, Thuringia’s
Infrastructure Minister
Susanna Karawanskij welcomed the new express
train.
The new RE 29 line (Nuremberg – Bamberg –
Coburg – Erfurt) is the
first change-free local transport connection between the Franconian city of Nuremberg
and the Thuringian state capital of Erfurt. The new line now takes passengers
from Nuremberg to Erfurt in 1 hour 53 minutes, cutting the travel time between
the two cities by half.
Even more impressive
is the time saved by passengers traveling between Coburg and Erfurt. They now
need only 36 minutes and no longer have to change trains for the regional
service. In the past, local passengers needed just over three hours and had to
make two changes for the same journey.
Christian Bernreiter,
Bavarian State Minister for Housing, Construction and Transport:
“The new service is a real winner and is sure to be a
great hit – especially as it can be used with inexpensive and convenient local
transport fares such as the Deutschlandticket (the country-wide Germany Ticket).
All passengers will be pleased, from local commuters to day trippers and even
business travelers. That’s why the funds provided by the Free States of Bavaria
and Thuringia are a good investment. I’m especially pleased that we are
providing even more local and regional service as part of the important German
Unity transport project. It shows that this high-speed rail line, which was
promoted by previous federal governments, is also incredibly valuable for local
and regional traffic and for further enhancing the quality of a location,
especially for regions like Coburg. This will make the VDE 8.1 an even better
model for success!”
Susanna Karawanskij, Thuringian Minister for
Infrastructure and Agriculture:
“Working in Erfurt, the evening off in Coburg, attending a concert in Nuremberg
on the weekend – and all with regional transport? With the inauguration of the
Franconia-Thuringia Express on June 9, all this is now possible – and with
regional transport that is almost as fast as the ICE. The new trains run from
Erfurt to Coburg in 36 minutes and to Nuremberg in just under two hours – and
at attractive prices, even with the Germany Ticket. Highly comfortable,
environmentally friendly, and inexpensive travel without traffic jams is
increasingly becoming a reality, and now also includes WiFi service,
state-of-the-art passenger information, and generous space for bicycles. The
new Franconia-Thuringia Express is bringing our regions closer together and
making them part of our collective homeland. And southern Thuringia is also
benefiting from the faster connections. I would like to thank Bayerische
Eisenbahngesellschaft in particular for its strong commitment to this project.”
Heiko Büttner, DB
Representative for the Free State of Bavaria:
“The inauguration
of the Franconia-Thuringia Express on the Nuremberg-Erfurt high-speed line
marks the opening of a new chapter in cross-border local and regional rail passenger
transport between Bavaria and Thuringia. This first direct connection in local
transport between Nuremberg/Coburg and Erfurt marks a truly quantum leap in
service. The new six-car trains provide 3,000 more seats every day, which will
especially benefit our passengers on the busy Nuremberg-Bamberg route. We can
now offer people in northern Franconia even better and significantly expanded
local service with many travel options to both the north and south.”
Karl Blaim, Managing
Director and Chief Financial Officer of Siemens Mobility:
“We are delighted to
officially hand over our six-car Desiro HC trains to Deutsche Bahn for the
timetable change. With a top speed of 190 km/h, they are among the fastest
regional trains in Germany. Not only do they operate safely with the modern
European Train Control System, but they also provide the highest level
of comfort and convenience with features like special high-frequency windows
for better mobile phone reception, a modern passenger information system, and
space for up to 60 bicycles.”
The new Desiro HC: High-speed service on the
VDE 8.1
Siemens Mobility has redesigned eight six-car Desiro HC double-decker trains specifically for use on the VDE 8.1 line. The new trains run at high speeds, are pressure-tight for passing other trains in tunnels and are equipped with the modern European Train Control System, which provides advanced control and safety technology for Germany’s rail system. Like the 18 four-car Desiro HC trains that entered service for the FTX back in December, the new six-car trains are equipped with WiFi service, advanced passenger information displays, large multi-purpose areas, and special windows that provide optimal mobile phone reception. The new trains can accommodate 634 passengers and up to 60 bicycles.
Siemens Mobility has redesigned eight six-car Desiro HC double-decker trains specifically for use on the VDE 8.1 line. The new trains run at high speeds, are pressure-tight for passing other trains in tunnels and are equipped with the modern European Train Control System, which provides advanced control and safety technology for Germany’s rail system. Like the 18 four-car Desiro HC trains that entered service for the FTX back in December, the new six-car trains are equipped with WiFi service, advanced passenger information displays, large multi-purpose areas, and special windows that provide optimal mobile phone reception. The new trains can accommodate 634 passengers and up to 60 bicycles.
More frequent and
faster – new rail routes, also with the Germany Ticket
Beginning with the scheduled so-called small timetable change, people in northern Bavaria are benefiting from further improvements in service, particularly in the Coburg area. Twice as many express trains now run from Coburg and Sonneberg to Nuremberg (RE 19) without transfers, providing 16 trains per direction between Coburg and Nuremberg every day. As a result, travel routes, such as between Coburg and the state capital Munich, are now much faster. The five pairs of trains operating on the RE 29 line supplement Coburg’s ICE connection to two-hourly service northwards, enabling travelers to get to Berlin or Frankfurt, for example, faster and more frequently.
Beginning with the scheduled so-called small timetable change, people in northern Bavaria are benefiting from further improvements in service, particularly in the Coburg area. Twice as many express trains now run from Coburg and Sonneberg to Nuremberg (RE 19) without transfers, providing 16 trains per direction between Coburg and Nuremberg every day. As a result, travel routes, such as between Coburg and the state capital Munich, are now much faster. The five pairs of trains operating on the RE 29 line supplement Coburg’s ICE connection to two-hourly service northwards, enabling travelers to get to Berlin or Frankfurt, for example, faster and more frequently.
Deutsche Bahn launched
service of 18 four-car Desiro HC trains on the Franconia-Thuringia Express at
the last timetable change in December 2023, enabling continuous half-hourly
service between Nuremberg and Bamberg every day.
Further information
Deutsche Bahn has published all information on the commissioning of the four-car Desiro HC trains in December 2023 in the following press release: https://www.deutschebahn.com/de/presse/presse-regional/pr-muenchen-de/aktuell/presseinformationen/Franken-Thueringen-Express-startet-mit-hochmodernen-Siemens-Zuegen-durch--12353534
Deutsche Bahn has published all information on the commissioning of the four-car Desiro HC trains in December 2023 in the following press release: https://www.deutschebahn.com/de/presse/presse-regional/pr-muenchen-de/aktuell/presseinformationen/Franken-Thueringen-Express-startet-mit-hochmodernen-Siemens-Zuegen-durch--12353534
Deutsche
Bahn has further information about the Franconia-Thuringia Express and facts
about the new trains available on its website.
The Franconia-Thuringia Express:
https://regional.bahn.de/regionen/bayern/ueber-uns/wir-und-unsere-partner/franken-thueringen-express
https://regional.bahn.de/regionen/bayern/ueber-uns/wir-und-unsere-partner/franken-thueringen-express
Note to
editors:
Photos of the event will be posted on the following websites: https://press.siemens.com/global/en/pressrelease/franconia-thuringia-express-sprints-siemens-trains-nuremberg-erfurt-high-speed-line https://mediathek.deutschebahn.com/marsDB/ko/de/7700166
Photos of the event will be posted on the following websites: https://press.siemens.com/global/en/pressrelease/franconia-thuringia-express-sprints-siemens-trains-nuremberg-erfurt-high-speed-line https://mediathek.deutschebahn.com/marsDB/ko/de/7700166
For this press release
Follow us on X
Siemens Mobility is a separately managed company of Siemens AG. As a leader in intelligent transport solutions for more than 175 years, Siemens Mobility is constantly innovating its portfolio. Its core areas include rolling stock, rail automation and electrification, a comprehensive software portfolio, turnkey systems as well as related services. With digital products and solutions, Siemens Mobility is enabling mobility operators worldwide to make infrastructure intelligent, increase value sustainably over the entire lifecycle, enhance passenger experience and guarantee availability. In fiscal year 2023, which ended on September 30, 2023, Siemens Mobility posted revenue of €10.5 billion and employed around 39,800 people worldwide. Further information is available at:
www.siemens.com/mobility
Contact
Silke Thomson-Pottebohm
Siemens Mobility Pressesprecherin
+49 1743063307