Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release13 November 2023Digital IndustriesNuremberg
TIA Portal Version 19: Motion control made easy for all users
Siemens' comprehensive motion control concept makes the interplay of engineering, control, and drives easy – for all users.
New features of the TIA Portal V19
In the TIA Portal, motion
control is intuitive and completely integrated, from engineering and control to
drives of machines and plants. Regardless of whether the user wants to control
a single axis or complex kinematics, the TIA Portal provides support with
graphical interfaces, intuitive technology objects, and extensive diagnostic
options like tracing. Version 19 brings even more enhancements: The new version
offers extended functions for improved engineering, including software units
that help with modularization. This allows different users to create their own
workspaces and write complex motion applications, among other things. These
modular areas make it easy to reuse applications, they’re easier to deploy,
track, and trace, and creating versions is also easier. The introduction of the
new engineering feature Named Values enables the creation of readable and
easy-to-maintain code as well as clear debugging, and this means greater
programming convenience for users. The enhancements in TIA Portal V19 also
support the use of SIMATIC CPUs for high-end applications in important segments
of mechanical engineering. They also enable the simulation of all types of
hardware and software controllers with S7-PLCSIM (Adv.).
Simatic Motion Interpreter
Siemens masters the
challenge created by the shortage of skilled workers in automation with the
Simatic Motion Interpreter software, which is integrated in the TIA Portal. The
Simatic Motion Interpreter doesn’t require in-depth programming knowledge; it
acts more like a navigation system, where the user enters a simple sequential
description of the movements that should be performed. The Simatic Motion
Interpreter then takes over the programming of the corresponding motion order. From
a single axis to complex kinematics with up to six interpolating axes. The
Simatic
S7-1500 T-CPU uses software to operate as a simple, integrated robot
controller.
Sinamics drive generation
The new generation of
Sinamics drives – suitable for use with delta pickers, for example – completes Siemens'
comprehensive motion control concept. Depending on the application, the drives
offer a variety of advantages. For example, the compact and precise Sinamics
S200 is fully integrated into TIA Portal and therefore very easy to engineer.
The Sinamics S210 offers safety functions up to Safety Integrity Level 3, and
the Sinamics G220 sets a new benchmark for energy efficiency thanks to 95
percent less harmonic distortion. Using a digital twin of the drives via
Sinamics DriveSim Basic and Advanced, tests and optimizations can be performed
in the virtual world.
This press release as
well as further information on Siemens at SPS are available at www.siemens.com/presse/sps23
Find further
information on TIA Portal at
www.siemens.de/tia-portal
www.siemens.de/tia-portal
For this press release
Follow us on our social media channels
Siemens Digital Industries (DI) is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI’s unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has around 72,000 employees internationally.
Siemens AG (Berlin and Munich) is a technology company focused on industry, infrastructure, transport, and healthcare. From more resource-efficient factories, resilient supply chains, and smarter buildings and grids, to cleaner and more comfortable transportation as well as advanced healthcare, the company creates technology with purpose adding real value for customers. By combining the real and the digital worlds, Siemens empowers its customers to transform their industries and markets, helping them to transform the everyday for billions of people. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a globally leading medical technology provider shaping the future of healthcare. In addition, Siemens holds a minority stake in Siemens Energy, a global leader in the transmission and generation of electrical power.
In fiscal 2022, which ended on September 30, 2022, the Siemens Group generated revenue of €72.0 billion and net income of €4.4 billion. As of September 30, 2022, the company employed around 311,000 people worldwide. Further information is available on the Internet at www.siemens.com.
In fiscal 2022, which ended on September 30, 2022, the Siemens Group generated revenue of €72.0 billion and net income of €4.4 billion. As of September 30, 2022, the company employed around 311,000 people worldwide. Further information is available on the Internet at www.siemens.com.