Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Siemens expands 3WA circuit breaker series to lead next generation electrical distribution

SENTRON 3WA UL air circuit breaker

As a core element of low-voltage switchboards, ACBs reliably protect electrical installations in buildings, infrastructure and industrial facilities from damage caused by short circuits, ground faults or overload faults. This is essential also for critical infrastructure, such as hospitals or data centers. The Sentron 3WA circuit breaker follows the Siemens tradition of high reliability ACBs that are built to perform over the lifetime of a facility. At the same time, the Sentron 3WA circuit breakers support software-based planning and engineering, digital testing and monitoring, and seamless integration in automation and IoT systems. Upgrades can be completed 100 percent digitally. Users simply download new features from the Internet and add them using an app. 
“Our highly flexible ACB series perfectly addresses the needs of switchgear manufacturers and panel builders in an environment characterized by increasing complexity, digitalization, and cost pressures,” said Andreas Matthé, CEO of Electrical Products at Siemens Smart Infrastructure.  
When technological requirements change, it is easy to add new features to the electronic trip unit (ETU600) installed in the Sentron 3WA air circuit breakers using the Sentron “powerconfig” commissioning software and a USB or communication port. The features are available online and are continually expanded by Siemens. Users benefit from high investment protection. For applications without a need for measuring functions or scaling options, the Sentron 3WA ACBs can now also be configured with an ETU300 for easy standard protection.  
The Sentron 3WA ACB trip units also have more standard features, such as the integrated arc energy reduction feature (Dynamic Arc Flash Sentry, DAS+), which ensures that Sentron 3WA ACBs trip more rapidly in the event of a fault during work being carried out in the immediate vicinity of live parts. In this way, the arc energy and thus the energy released in the power distribution equipment room is reduced. This technology complies with the National Electric Code (NEC) for the US market; it is designed to protect service technicians from serious injury resulting from arc flash hazards. 
The Sentron 3WA ACB UL series 3WA2 and 3WA3 are available in three frame sizes with rated current ranges from 800 to 5,000 A.  
For more information about Siemens´ Sentron 3WA air circuit breakers, see www.siemens.com/3wa

SENTRON 3WA UL air circuit breaker

For this press release

Press Folders

Follow us on Twitter

Siemens Smart Infrastructure (SI) is shaping the market for intelligent, adaptive infrastructure for today and the future. It addresses the pressing challenges of urbanization and climate change by connecting energy systems, buildings and industries. SI provides customers with a comprehensive end-to-end portfolio from a single source – with products, systems, solutions and services from the point of power generation all the way to consumption. With an increasingly digitalized ecosystem, it helps customers thrive and communities progress while contributing toward protecting the planet. Siemens Smart Infrastructure has its global headquarters in Zug, Switzerland. As of September 30, 2022, the business had around 72,700 employees worldwide.
Read more
Siemens AG (Berlin and Munich) is a technology company focused on industry, infrastructure, transport, and healthcare. From more resource-efficient factories, resilient supply chains, and smarter buildings and grids, to cleaner and more comfortable transportation as well as advanced healthcare, the company creates technology with purpose adding real value for customers. By combining the real and the digital worlds, Siemens empowers its customers to transform their industries and markets, helping them to transform the everyday for billions of people. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a globally leading medical technology provider shaping the future of healthcare. In addition, Siemens holds a minority stake in Siemens Energy, a global leader in the transmission and generation of electrical power.
In fiscal 2022, which ended on September 30, 2022, the Siemens Group generated revenue of €72.0 billion and net income of €4.4 billion. As of September 30, 2022, the company had around 311,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Read more

Contact

Christian S. Wilson

Siemens AG

+49 172 138 5608