Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Siemens launches one of the most efficient DC chargers currently available on the market

The new public charger of Siemens Sicharge D is suited for highway and urban fast charging stations, city parking as well as shopping malls.

“With its upgradability and dynamic charging, it is a big step forward to support the future of eMobility. Our customers can be sure to be prepared for future eventualities of eMobility, be it increasing number of required charging options or increasing charging speeds,” said Birgit Dargel, Global Head of Future Grids at Siemens Smart Infrastructure. “At the same time, it is one of the most efficient fast chargers currently available on the market – an important aspect since building sustainable mobility requires careful handling of the scarce resources we are using.”
With a constant efficiency of above 95.5 percent and a peak efficiency of 96 percent, the new Sicharge D ensures that almost all of the generated electricity reaches the car to be charged. For customers this means reduced operational costs. In addition, the charger is designed to meet future technological developments: Even if the charging capacities of most electric vehicles are still limited today, they will be able to accept higher charging power in the future and demand higher voltage ranges. Therefore, the Sicharge D has a scalable charging power up to 300 kW, either from the start or through plug-and-play upgrades. Furthermore, the charger already supports voltages between 150 and 1,000 volts (V) and currents of up to 1,000 amperes (A) across all DC outlets. This enables full power loads for future 800 V vehicles as well as the lower voltage charging rates demanded by todays mainstream vehicles.
Although the number of electric vehicles is growing, today's investments in infrastructure are challenging. With the option to expand the Sicharge D with up to two external dispensers, it is possible for customers to time the investments according to market demands. The standard configuration has two DC and one AC outlet housed in a compact design that minimizes installation complexity. 
The new charger combines all these features with dynamic parallel charging. That means, it accounts for the individual power demand of each connected car and automatically adapts the charging process to the EV's battery technology and charging status. This ensures that the connected cars get the maximum power they need without any additional manual intervention. 
For an improved user experience, an integrated 24-inch adjustable display allows to easily operate the Sicharge D charger barrier-free and opens new opportunities for customers to use the chargers display for tasks beyond interfacing with the charging process. 
This press release as well as press photos can be found at
https://sie.ag/2WDpk2M
For more information about Sicharge D, see
www.siemens.com/sicharge-D
For more information about Siemens Smart Infrastructure, see
www.siemens.com/smart-infrastructure

For this press release

Press Folders

Follow us on Twitter

Siemens Smart Infrastructure (SI) is shaping the market for intelligent, adaptive infrastructure for today and the future. It addresses the pressing challenges of urbanization and climate change by connecting energy systems, buildings and industries. SI provides customers with a comprehensive end-to-end portfolio from a single source – with products, systems, solutions and services from the point of power generation all the way to consumption. With an increasingly digitalized ecosystem, it helps customers thrive and communities progress while contributing toward protecting the planet. SI creates environments that care. Siemens Smart Infrastructure has its global headquarters in Zug, Switzerland, and has around 72,000 employees worldwide.
Read more
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. Active around the world, the company focuses on intelligent infrastructure for buildings and distributed energy systems and on automation and digitalization in the process and manufacturing industries. Siemens brings together the digital and physical worlds to benefit customers and society. Through Mobility, a leading supplier of intelligent mobility solutions for rail and road transport, Siemens is helping to shape the world market for passenger and freight services. Via its majority stake in the publicly listed company Siemens Healthineers, Siemens is also a world-leading supplier of medical technology and digital health services. In addition, Siemens holds a minority stake in Siemens Energy, a global leader in the transmission and generation of electrical power that has been listed on the stock exchange since September 28, 2020. In fiscal 2020, which ended on September 30, 2020, the Siemens Group generated revenue of €57.1 billion and net income of €4.2 billion. As of September 30, 2020, the company had around 293,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Read more

Contact

Anna Korb

Siemens AG

+49 9131 173 663 7