Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Siemens enables climate-neutral, safe energy distribution with new Clean Air switchgear

The F-gas-free Clean Air switchgear NXPLUS C 24  extends the Siemens blue GIS portfolio to 24 kV level and has integrated sensors and communications interfaces to higher-level automation and the Internet of Things (IoT) systems.

Sustainability already plays a major role in energy generation. According to Strom-Report.de, nearly half of the electricity generated in Germany in 2019 was from renewable sources. “When electrical energy is generated in an environmentally-friendly manner, transmission and distribution need to follow suit. Switchgear are key components for a safe, reliable and efficient energy distribution in all grid structures, and therefore play an important role in infrastructures of today and tomorrow,” said Stephan May, CEO of the Distribution Systems Business Unit at Siemens Smart Infrastructure.
The new gas-insulated switchgear is part of the blue GIS portfolio from Siemens. In the NXPLUS C 24 a vacuum-interrupter unit switches and extinguishes the arc, while Clean Air provides the insulation for the current-carrying conductors inside the hermetically sealed interior of the switchgear housing. This insulation medium consists only of the natural constituents of ambient air, such as nitrogen or oxygen. As a result, no special equipment is required, unlike when using F-gases or F-gas mixtures. An easy management of the switchgear can be assured over its entire life cycle. Furthermore, it eliminates the mandatory reporting of the gas quantities used and emissions produced.

The NXPLUS C 24 is the third medium-voltage switchgear from the Siemens blue GIS portfolio and the first with a rated voltage up to 24 kV (left). A ring-main unit (RMU) with the same rated voltage will join the blue GIS family as the next new member (right).

The switchgear is used in public and industrial grids at the primary distribution level to feed energy from the transmission into the distribution grid. Distribution grid structures and switchgear must also adapt to the requirements resulting from increasingly decentralized renewable energy sources and prosumers. The result is that power flows are getting more complex, bidirectional, and harder to control. Like all switchgear in the blue GIS portfolio, the new NXPLUS C 24 has integrated sensors and communications interfaces to higher-level automation and the Internet of Things (IoT) systems. This increases transparency over all relevant nodes in the distribution grid and makes energy distribution easier to monitor and control while enhancing cost efficiency. 
The blue GIS portfolio from Siemens retains all the proven benefits of traditional, gas-insulated switchgear, including compact size, reliability, long service life, and maintenance-free operation. After the 8DAB 12 and 8DJH 12 switchgear models with a rated voltage up to 12 kV, which are already in use at customer installations, the NXPLUS C 24 is the third medium-voltage switchgear from the Siemens blue GIS portfolio and the first with a rated voltage up to 24 kV. A ring-main unit (RMU) with the same rated voltage will join the blue GIS family as the next new member.
Registration for blue GIS webcast 
https://www.beamstream-hd.com/blueGIS/  
For more information about Siemens NXPLUS C 24, see
www.siemens.com/nxplusc24
For more information about the Siemens blue portfolio, see https://new.siemens.com/global/en/products/energy/ecotransparency.html
For more information about Siemens Smart Infrastructure, see
www.siemens.com/smart-infrastructure  
Siemens Smart Infrastructure (SI) is shaping the market for intelligent, adaptive infrastructure for today and the future. It addresses the pressing challenges of urbanization and climate change by connecting energy systems, buildings and industries. SI provides customers with a comprehensive end-to-end portfolio from a single source – with products, systems, solutions and services from the point of power generation all the way to consumption. With an increasingly digitalized ecosystem, it helps customers thrive and communities progress while contributing toward protecting the planet. SI creates environments that care. Siemens Smart Infrastructure has its global headquarters in Zug, Switzerland, and has around 72,000 employees worldwide.
Read more
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of intelligent infrastructure for buildings and distributed energy systems, and automation and digitalization in the process and manufacturing industries. Through the separately managed companies Siemens Energy, the global energy business of Siemens, and Siemens Mobility, a leading supplier of smart mobility solutions for rail and road transport, Siemens is shaping the energy systems of today and tomorrow as well as the world market for passenger and freight services. Due to its majority stakes in the publicly listed companies Siemens Healthineers AG and Siemens Gamesa Renewable Energy (as part of Siemens Energy), Siemens is also a world-leading supplier of medical technology and digital healthcare services as well as environmentally friendly solutions for onshore and offshore wind power generation. In fiscal 2019, which ended on September 30, 2019, Siemens generated revenue of €86.8 billion and net income of €5.6 billion. At the end of September 2019, the company had around 385,000 employees worldwide. Further information is available on the Internet www.siemens.com.
Read more

Contact

Anna Korb

Siemens AG

Freyeslebenstr. 1
91058 Erlangen 
Germany

+49 (9131) 173 663 7