Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Sicharge UC system sets new standards for flexible eBus charging

The number of electric vehicles in the bus and logistics environment continues to grow and is becoming an increasingly important factor for fleet operators. Taking this into consideration, it becomes increasingly important for them to be able to charge vehicles from multiple manufacturers. At the same time, the charging process should be optimally integrated in their day-to-day operations. The Sicharge UC portfolio is compatible with the Combined Charging System (CCS) charging standard, ensuring that charging processes are vendor-neutral. It is also available in power levels from 50 to 600 kW, which means operators get the most out of their depots by charging various vehicle types such as buses and trucks.
The charging system is also flexible with regards to its application. “For buses that cover a lengthy route during the day, for example, a single charge at the depot is often not enough,” said Monique Mertins, Head of Charging Infrastructure Europe and Latin America at Siemens Smart Infrastructure. “Additional charging points are needed along the route. That’s why it’s important that charging stations can be connected to various contact systems like charging plugs, which are often used for depot charging, and also to pantographs for charging at other points along the way. The advantage of a pantograph is, that the vehicle will connect with the charging system entirely automatically, with no need to attach a plug manually.”

The Sicharge UC system can be combined with several connection options like charging plugs and offboard or onboard pantographs.

The compact size of the charging stations and the pantographs of the UC family means they can be integrated into existing depots and external infrastructure without taking up much space.
With the Sicharge UC portfolio, a cloud-based application can take over the monitoring and controlling of the charging processes to make them as efficient as possible. For example, it can apply “smart charging” principles to ensure the system charges only when the electricity price is favorable, or that the depot doesn’t exceed a set maximum power level.
With the increasing number of electric vehicles, the size of depots is also growing. Such infrastructures with high energy capacity will put tremendous challenges to the power supply from the grid. „To provide reliable and cost-efficient smart charging infrastructures it will be important in the future to combine charging systems, as Sicharge UC, with battery energy storage systems and an application for intelligent load management,” said Jean-Christoph Heyne, Global Head of Future Grids at Siemens Smart Infrastructure.
Sicharge UC charging stations with a capacity of 150 kW are already in use at the Charging Test Center of the Dutch bus manufacturer VDL Bus & Coach (VDL) in Valkenswaard. Siemens and VDL have joined efforts to come up with innovative solutions for depots charging.
For further information on Siemens Smart Infrastructure, please see
www.siemens.com/smartinfrastructure

For further information on Sicharge UC, please see
www.siemens.com/sichargeuc
Siemens Smart Infrastructure (SI) is shaping the market for intelligent, adaptive infrastructure for today and the future. It addresses the pressing challenges of urbanization and climate change by connecting energy systems, buildings and industries. SI provides customers with a comprehensive end-to-end portfolio from a single source – with products, systems, solutions and services from the point of power generation all the way to consumption. With an increasingly digitalized ecosystem, it helps customers thrive and communities progress while contributing toward protecting the planet. SI creates environments that care. Siemens Smart Infrastructure has its global headquarters in Zug, Switzerland, and has around 71,000 employees worldwide.
Read more
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2018, which ended on September 30, 2018, Siemens generated revenue of €83.0 billion and net income of €6.1 billion. At the end of September 2018, the company had around 379,000 employees worldwide. Further information is available on the Internet at www.siemens.com .
Read more

Contact

Anna Korb

Smart Infrastructure

Freyeslebenstr. 1
91058 Erlangen
Germany

+49 (9131) 17-36637