Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser
Charger locomotive for Illinois Department of Transportation (IDOT)
In 2014, the Departments of Transportation of California, Illinois and Maryland ordered an initial lot of 34 Charger locomotives from Siemens, with an option for a total of 222 locomotives. The contract back then was valued at approximately €165 million ($225 million). Due to orders from other states as well as by the private rail operator All Aboard Florida, the total number of Chargers ordered amounts to 81 in 2017. The locomotives are deployed in corridors of the US states for regional and mainline trains travelling for Caltrains (California) as Amtrak Pacific Surfliner, in Washington as Amtrak Cascades and in Maryland with the regional network MARC. Under the "Brightline" brand, ten Chargers are being deployed in high-speed rail services between Miami and West Palm Beach; Orlando is due to follow at a later date.

Press Pictures

Most environmentally friendly diesel locomotive for high-speed transport in the USA

In 2014, the Departments of Transportation of California, Illinois and Maryland ordered an initial lot of 34 Charger locomotives from Siemens, with an option for a total of 222 locomotives. Due to orders from other states as well as by the private rail operator All Aboard Florida, the total number of Chargers ordered amounts to 81.

On tour deployed in corridors of the U.S.

The locomotives are deployed in corridors of the U.S., including Illinois (in the picture), by Caltran (California) as Amtrak Pacific Surfliner, in Washington as Amtrak Cascades and in Maryland with the regional network operator MARC.

Videos

Test driving of the charger locomotives by Siemens
Video Player is loading.
Current Time 0:00
Duration 0:00
Loaded: 0%
Stream Type LIVE
Remaining Time 0:00
 
1x
    • Chapters
    • descriptions off, selected
    • captions off, selected

      Test driving of the charger locomotives by Siemens

      A variety of tests and validation exercises including maximum speed runs, acceleration and braking and the overall performance capabilities of the locomotive are conducted to ensure it is operating and performing as designed.

      Further Information

      Contact

      Eva Haupenthal

      Siemens Mobility GmbH

      +49 152 01654597