Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release19 April 2017Process Industries and DrivesNuremberg
High-performance Simotics DP roller table motor for extreme conditions
The picture shows the Simotics DP roller table motor from Siemens.
The standard versions of the Simotics DP roller table motors are classified in compliance with protection rating IP66. They can optionally be fitted with an additional "special sealing system – corrosion protection" to withstand exceptionally tough environmental conditions. Their vibration and shock resistance is tested and confirmed in exhaustive test lab trials.
The series is based on the new motor platform 1LE1 and is designed to supplement the existing Simotics DP steel mill motors in sizes 112M-200L, making this a one-stop solution for all kinds of transport applications in the metalworking industry. This not only reduces any associated risks but also makes for more efficient project engineering.
Simotics DP roller table motors are ideally suited for operation in conjunction with the SINAMICS S120 converter. Operation of this combined system has been exhaustively laboratory tested.
For further information on topic Simotics DP, please see www.siemens.com/simotics-dp
For further information on Siemens at the Hannover Messe 2017, please see www.siemens.com/press/hm17 and www.siemens.com/hannovermesse
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Stefan Rauscher
Siemens AG
Gleiwitzer Str. 555
90475 Nuremberg
Germany
90475 Nuremberg
Germany
+49 (911) 895-7952