Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release20 February 2017Energy ManagementErlangen
Siemens drives new advances in process bus communication for energy automation
The global trend toward digitalization is also finding its way into time-critical applications such as electrical power supply. However, it is only through the use of new communications processes such as process bus technology that it has become possible to ensure adequate performance in terms of availability, time response and data security. In energy automation, for example, ethernet-based communication processes have become the established "state-of-the-art" technology. The international standard IEC61850 in particular has played an important role as the communications standard for station automation because it takes all aspects relating to the power supply – such as data exchange, availability and interoperability – into account.
With ethernet-based communication, the process bus now also dominates the lower level in energy automation, which is referred to as the process level. This means that not only messages but also the current and voltage measured values from sensors, for example current and voltage transducers, are transmitted digitally over the Ethernet to the protection device or monitoring system. In this context, the communications standards IEC61850-9-2 (Process bus) and IEC 62439-3 (PRP/HSR Redundancy protocols) form the basis for the necessary high availability and precision timing of data transmission at process level.
The trend toward greater digitalization is not only technology-driven; on the contrary, it is creating possibilities for realizing new ideas and concepts that offer more than the previously used technologies for everyone involved. This includes, for example, increased availability, greater security and lower costs throughout the entire system lifecycle. As one of the market leaders and trendsetters in the field of energy automation, Siemens is continuously working on new technologies and concepts so that power supply systems can be operated at optimum efficiency. That's why Siemens is one of the first manufacturers investing in process bus technology and driving new advances.
For further information on Division Energy Management, please see www.siemens.com/energy-management
For this press release
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Reference Number: PR2017020174EMEN
Contact
Dietrich Biester
Siemens AG
Freyeslebenstr. 1
91058 Erlangen
Germany
91058 Erlangen
Germany
+49 (9131) 7-33559