Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Innovative design concept for Simotics HV C

The picture shows the high-voltage motors of the Simotics HV C series

The outstanding performance density and rugged durability of these new motors are due to a range of innovative design measures and a modern housing concept optimized using the Finite Element Method (FEM).
In the cooling concept of the air-cooled flameproof variants, elements of the tube cooling have been integrated into the fin-cooled housing, bringing about a marked improvement in cooling performance, particularly of hotspots. At the same time, a modern fan design with internal coolant circuit helps additionally optimize heat dissipation. The water jacket-cooled variant has also benefitted from an innovated cooling concept which has significantly improved temperature distribution and heat dissipation. These measures have meant improved reliability and durability in both variants.
Design measures have also been implemented to improve the foot structure of the rugged housing for optimized vibration behavior. The flow-optimized fan cover design has reduced noise generation without compromising performance.
The flameproof terminal box of the Simotics HV C is designed for maximum compactness and is identical for both the 6 kilovolt (kV) and 11 kV version, with weight savings of up to several hundred kilograms. The flexibility afforded by the variable position of the terminal box helps simplify plant planning and installation. Internal cable ducts make the motor resistant to even the harshest of conditions and also help to reduce cabling work. The concept of integrated cabling shields the cables from all kinds of external influences.
The high-grade standardization of production processes and interfaces in the Simotics HV C and its integration into the whole range of available marketing and engineering tools help cut delivery times relative to performance.

For further information on topic Simotics HV C, please see www.siemens.com/simotics-hv-c
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Read more

Contact

Stefan Rauscher

Siemens AG

Gleiwitzer Str. 555
90475 Nuremberg
Germany

+49 (911) 895-7952