Siemens will be responsible for the design, engineering, supply, installation, and commissioning of the substations for the 400-kilovolt (kV), 220-kV, 132-kV, 66-kV, and 11-kV voltage levels, including gas-insulated switchgear, transformers, and control and protection equipment. Since the upgrade program started in 2005, Siemens has installed more than 120 substations and approximately 1,500 kilometers of high-voltage cable. With this new order intake, our completed and under execution projects with KAHRAMAA total nearly EUR2.5 billion.
"We are delighted to build on a trusting relationship with KAHRAMAA, as we embark on yet another important phase to upgrade Qatar's power network. Siemens is committed to supplying reliable and innovative products to this highly ambitious project that will meet growing demand for electricity in a fast-developing country," said Ralf Christian, CEO of Siemens Energy Management Division.
As part of this contract, an existing 'super substation' – one that allows multiple voltage settings – in Doha will be upgraded with new 400kV/200kV gas-insulated switchgear and associated equipment, before connecting to the grid. Another substation will be used to meet rising demand for electricity in Al Jahhaniya and surrounding area, including temporary power feed to Rayyan Stadium, one of the venues for the upcoming world soccer championship. Substations will also feed power to steel, oil and gas and petrochemical facilities in Mesaieed industrial area, as well as Al Sadd area in Doha. Overall, the substations are required to supply power for ongoing infrastructure development projects, schools, hospitals, industries and residential complexes in and around Doha, Qatar's capital city.
In addition to Phase 13, Siemens also received a second order from KAHRAMAA to supply and install more than 2,170 medium-voltage switchgear boards. The 8DJH switchgear will be used as ring main units (RMU) in the 11 kV distribution network. RMUs protect, for example, transformers connected to the grid against overloads and short-circuits, ensuring a reliable power supply. The switchgear will be manufactured in Frankfurt, with the first units expected to go into operation by end-2017. The order is valued at roughly EUR27 million.
Demand for electricity in Qatar has been steadily rising over the past decade, thanks to its growing population and a government strategy that seeks to develop various sectors of the economy and reduce reliance on hydrocarbons. As a local company that has been operating in the Qatari market for more than four decades, Siemens has almost 500 employees in the country and contributes to transmitting and distributing more than 60 percent of the power generated there. Its partnership with KAHRAMAA dates back to 2005 when the utility was founded. Siemens is currently executing an order valued at EUR470 million to deliver 18 turnkey substations for KAHRAMAA's Phase 12, part of its plans to expand its power transmission network. KAHRAMAA has closely aligned its strategy with the Qatar National Vision 2030. Phase 13 of the Qatar Power Transmission System Expansion project is due for completion by 2020, helping the country prepare for hosting major sports events in 2022.