Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release11 September 2017Energy ManagementErlangen
First use of new Siemens railway transformers in the Rhine valley network of DB Regio

The picture shows the transformer type Tractronic® Thinity
"Through the use of new materials and thanks to our innovative cooling concept, the Tractronic® Thinity is a real lightweight," said Beatrix Natter, CEO of Siemens Power Transformers. "With a weight saving of up to 25 percent, we've also been able to further reduce losses. That makes the Tractronic® Thinity the most efficient and flexible vehicle transformer on the market."
Energy efficiency and flexibility are the key factors in operation. The improved efficiency of the transformers and the lightweight construction of the Mireo also reduce the energy consumption of the train by 25 percent. Because of its flexible design, the new train transformer can not only be roof-mounted but also installed underfloor, offering the operator the greatest possible flexibility. Various optimization measures on the active components, such as a special coating on the iron core, allow especially compact construction of the transformer. A groundwater-neutral and biologically degradable ester oil is used as insulation and as a cooling medium. The cooling concept has been optimized by the use of state-of-the-art 3D-CFX simulations, so that the use of coolant is reduced to a minimum. This not only has a positive impact on the weight but also significantly improves fire protection.
Traction transformers provide the power supply to all areas of a rail vehicle, and are thus essential for the proper functioning of, for example, brakes and traction unit. They also ensure the function of lighting and ventilation systems as well as signaling technology and communications systems. Siemens is a leading manufacturer of traction transformers which are employed in all parts of the world. Production at five global Siemens locations under the lead management of the center of expertise in Nuremberg guarantees highest quality and reliability for trouble-free operation over many years.
For further information on Division Energy Management, please see www.siemens.com/energy-management
For further information on railway transformers, please see www.siemens.com/transformers
For this press release
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Reference Number: PR2017090420EMEN
Contact
Sabrina Martin
Siemens AG
Freyeslebenstr. 1
91058 Erlangen
Germany
91058 Erlangen
Germany
+49 (9131) 7-37168