Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release28 November 2017Process Industries and DrivesNuremberg
Dedicated safety system design made easy using Simatic SIS compact
Safety applications such as Burner Management Systems (BMS), Emergency Shutdown Systems (ESD), Fire&Gas (F&G) applications as well as High Integrity Pressure Protection Systems (HIPPS) can be achieved easily and safely using the Simatic SIS compact.
The basic hardware is a CPU 410SIS controller. The software package uses Simatic S7 F systems and ensures that safety-oriented, fault-tolerant and standard programs can run on the same CPU.
For an optimum match to specific safety requirements, the Simatic SIS compact system is available in four pre-configured bundles. Basic and Extended packages, each in a Single and Redundancy version. They can be connected to any process control system via Modbus/TCP. The two so-called extended packages contain additional OS software for HMI functions, such as the Simatic Safety Matrix. Highly available systems with respect to the CPU, communication and distributed I/O systems can be created using the respective Redundancy-variant.
The TÜV certificated Safety Lifecycle Management Tool "Simatic Safety Matrix" allows safety applications up to SIL 3, in accordance with IEC 61508, to be used with the extended packages. It can be used for the engineering of safety applications as well as for their easy operation and monitoring.
For further information, refer to www.siemens.com/process-safety
Further information about Siemens at the SPS IPC Drives 2017 at
www.siemens.com/sps-ipc-drives and www.siemens.com/press/sps2017
For further information, refer to www.siemens.com/process-safety
Further information about Siemens at the SPS IPC Drives 2017 at
www.siemens.com/sps-ipc-drives and www.siemens.com/press/sps2017
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 372,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Evelyne Kadel
Siemens AG
Klaus-Bungert-Str. 6
40468 Duesseldorf
Germany
40468 Duesseldorf
Germany
+49 (211) 6916-1003