Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Converter handling simplified by new module for wireless commissioning

The composing shows the G120 Smart Access Module

The G120 Smart Access Module is available for Sinamics G120C, Sinamics G120 with Control Units CU230P-2 and CU240-E2, as well as for Sinamics G120P with CU230P-2. Since the use of the module is not linked to a specific web browser, customers are free to choose any preferred browser and use any optional terminal such as a smartphone, tablet or laptop for converter commissioning, parameterization and maintenance. The motor can also be tested in the JOG mode. Error messages or warning signals are quickly detected over the wireless link, which can also be used to save or reset settings. A function enabling the settings from one converter to be duplicated, sent to other mobile devices and used to set additional converters provides an enormous labor saving when handling several converters. It is also possible to swap Sinamics G120 Smart Access Modules between different converters of the specified series, allowing them to be commissioned using a single mobile terminal. In this case, the module acts as a transportable storage facility with web-based operator unit and wireless client link.
For further information on the Sinamics Smart Access Module please see www.siemens.com/sinamics-accessories
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 377,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Read more

Contact

Katharina Lamsa

Siemens AG

Gleiwitzer Str. 555
90475 Nuremberg
Germany

+49 (911) 895-7975