[{"name":"Home","site_name":"Press | Company | Siemens","description":"","url_str":"\/global\/","level":0,"image":"","base_root":"https:\/\/press.siemens.com","base_nid":"5","base_nodepath":"\/node\/5","base_path":"\/global\/","base_secure_url":"https:\/\/press.siemens.com\/global","children":null}]
It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and
usability.
For the best experience we suggest that you download the newest version of a supported browser:
Press Release16 April 2018Process Industries and DrivesNuremberg
Siemens industrial communication relies on Time-Sensitive Networking (TSN)
Robotic trade fair model demonstrates TSN communication between machine controls
Standardized interfaces for guaranteed quality of service
OPC UA PubSub with TSN: reliable communication even under high network load conditions
Network components, communication processors, software and network management
At Hannover Messe 2018, Siemens will be showcasing a trade fair model to demonstrate the advantages of Time-Sensitive Networking (TSN): TSN enables even more robust and reliable Ethernet communication between machines and plants even under high network load conditions. The model uses OPC UA PubSub (Publisher/Subscriber) together with TSN for machine-to-machine (M2M) communication. The reliability of TSN provides significant advantages for automation applications in industries such as automotive, mechanical engineering and food&beverage. The first Siemens products are expected to be available towards the end of 2018: network components, communication processors, software and network management with TSN functionality.
Robotic trade fair model demonstrates TSN communication between machine controls
Standardized interfaces for guaranteed quality of service
OPC UA PubSub with TSN: reliable communication even under high network load conditions
Network components, communication processors, software and network management
At Hannover Messe 2018, Siemens will be showcasing a trade fair model to demonstrate the advantages of Time-Sensitive Networking (TSN): TSN enables even more robust and reliable Ethernet communication between machines and plants even under high network load conditions. The model uses OPC UA PubSub (Publisher/Subscriber) together with TSN for machine-to-machine (M2M) communication. The reliability of TSN provides significant advantages for automation applications in industries such as automotive, mechanical engineering and food&beverage. The first Siemens products are expected to be available towards the end of 2018: network components, communication processors, software and network management with TSN functionality.
The advantages of Time-Sensitive Networking (TSN) on a trade fair model.
The trade fair model consists of two robots, each of which communicates over Profinet with a Simatic controller, and it demonstrates their synchronized motion. Synchronization between both controllers is ensured by the TSN network using a TSN-based OPC UA PubSub. The vital underlying element is the Publisher/Subscriber (PubSub) principle: A publisher such as a machine control sends data to the network, which is then available to all subscribers. The subscribers "decide" for themselves whether they require this information. Bandwidth reservation ensures data transmission within the TSN network in an exactly predictable form and irrespective of the network load.
The model applies the advantages of OPC UA with TSN: TSN combines the existing standards and optimizes Ethernet with an extended Quality of Service (QoS) mechanism, time synchronization, low transmission latencies and seamless redundancy. Users placing heavy demands on reliable communication will benefit particularly from the outstanding advantages of QoS prioritization: The reservation of a particular bandwidth and predictable latency periods ensures that each application is given the communication facilities it requires. The model also demonstrates the coexistence of TSN communication and standard Ethernet communication, whereby data is transmitted from the controller via a communication processor into MindSphere.
TSN has now reached the required degree of technical maturity (including standards), and the first components are available as a hardware basis. Siemens and other manufacturers are now able to extend their existing industrial networks to include new applications.
The next step involving Profinet based on TSN will be shown in a live demonstration to visitors at the PI booth (Profibus & Profinet International) in Hall 9, Booth D68 at Hannover Messe 2018.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 377,000 employees worldwide. Further information is available on the Internet at www.siemens.com.