Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release18 June 2018Digital Factory Nuremberg
All-round IP65 and IP66 protected HMI devices for operator control and monitoring
The all-round IP66 protected Simatic HMI Thin Client Ex OG is the new addition to the series of Ex HMI devices. It can be used in 1/21 and 2/22 zones without any special measures such as elaborate enclosures or additional certifications. The Ex OG HMI devices are specially designed for applications in industries such as chemicals, oil, gas and shipbuilding, and are suitable for use in extreme temperatures ranging from -40 C to +65 degrees Celsius.
The new Ex OG devices are complemented by material for four mounting types and equipment options such as cameras, Bluetooth, wireless and internal RFID(Radio Frequency Identification) readers.
For further information, refer to www.siemens.com/simatic-hmi-pro
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 377,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Gerhard Stauss
Siemens AG
Gleiwitzer Str. 555
90475 Nuremberg
Germany
90475 Nuremberg
Germany
+49 (911) 895-7945