[{"name":"Home","site_name":"Press | Company | Siemens","description":"","url_str":"\/global\/","level":0,"image":"","base_root":"https:\/\/press.siemens.com","base_nid":"5","base_nodepath":"\/node\/5","base_path":"\/global\/","base_secure_url":"https:\/\/press.siemens.com\/global","children":null}]
It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and
usability.
For the best experience we suggest that you download the newest version of a supported browser:
Press Release01 October 2018Energy ManagementErlangen
Siemens busbars receive DNV certificate
Conformity statement confirms high safety and reliability standards for use in wind turbines
System can now be used in photovoltaic systems thanks to expanded product family
The DNV GL classification company awarded Siemens the certificate for its busbar trunking system from the Sivacon 8PS product family at the international Wind Energy trade fair in Hamburg. The CS-03832 conformity statement confirms that the LDM system meets high standards of safety and reliability. Especially when it comes to high current intensities, busbar trunking systems are an excellent alternative to classic cable installations. The busbars can be installed in very limited space and ensure high availability and low maintenance. During operation, they feature low fire load and have a PVC and halogen-free design. The systems use solid aluminum as conductors, a material that costs much less than the copper used in cables. It can also easily be recycled after use.
Conformity statement confirms high safety and reliability standards for use in wind turbines
System can now be used in photovoltaic systems thanks to expanded product family
The DNV GL classification company awarded Siemens the certificate for its busbar trunking system from the Sivacon 8PS product family at the international Wind Energy trade fair in Hamburg. The CS-03832 conformity statement confirms that the LDM system meets high standards of safety and reliability. Especially when it comes to high current intensities, busbar trunking systems are an excellent alternative to classic cable installations. The busbars can be installed in very limited space and ensure high availability and low maintenance. During operation, they feature low fire load and have a PVC and halogen-free design. The systems use solid aluminum as conductors, a material that costs much less than the copper used in cables. It can also easily be recycled after use.
Left to right: Niels Nilsen (Sales Engineer, Siemens), Dr. Matthias-Klaus Schwarz (Head of Section Electrical Systems, DNV GL), Carsten Schwarz (Product Manager busbars, Siemens)
DNV GL is a quality assurance and risk management company that offers certification and independent consulting services by experts for the oil and gas industry, the energy sector, and the shipping industry. Driven by the goal of protecting life, property, and the environment, DNV GL gives companies the opportunity to improve the safety and sustainability of their business.
The busbar trunking systems in the Sivacon 8PS portfolio have been used successfully in wind turbines for several years. The LDM-P busbar trunking system has now been added to the product family. This system is destined for use in solar power plants where extremely high amounts of energy are transmitted in very limited space. The benefits of the technology over cable-based solutions are particularly apparent in this area. These include fast planning and installation, current intensities up to 7,000 amperes (A), and exact adaptation to other necessary products, such as inverters and transformers. Siemens also provides comprehensive support during the planning phase and enables the customer to achieve integrated and thus very efficient power distribution.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 377,000 employees worldwide. Further information is available on the Internet at www.siemens.com.