Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release13 May 2019Smart InfrastructureZug
Siemens presents solutions for a climate-friendly energy future
At the trade show, the company will present solutions and services for planning, installing and operating individual supply solutions based on renewable energy and intelligent energy management systems for buildings, infrastructure and industry. Attendees will also be able to learn all about systems and products for the grid integration of photovoltaic (PV) power plants, battery storage systems and charging infrastructure solutions for electromobility. Expert presentations on subjects including transforming the energy system, renewable energy sources and storage technologies will round out Siemens' exhibit at Booth 110 in Hall B2.
"We are supporting our customers to turn the challenges of the energy transition into business opportunities" says Cedrik Neike, Member of the Management Board of Siemens AG and CEO of Smart Infrastructure. "We are investing to shape the market at the grid edge: we have refreshed our portfolio of eMobility charging solutions; acquired power electronics leader, KACO new energy; and are consolidating our leadership in battery storage with our joint venture Fluence."
Connecting PV power plants securely to the grid
The rising trend toward generating power from renewable energy sources is presenting grids with new challenges, especially where stability is concerned. With its Photovoltaic eBoP (photovoltaic electrical balance of plant), Siemens offers a complete solution for reliably connecting PV power plants to the medium- or high-voltage grid. The package covers all the required electrical components including the PV SKid Outdoor platform, a comfortable, easy-to-install plug-and-play solution with switchgear, transformer and Sinacon PV inverters. The 1500V inverters have an especially high-power density and are suitable for use in large solar power plants, even under harsh environmental conditions. The LDM-P busbar trunking system from the Sivacon 8PS portfolio is designed specifically for the requirements of photovoltaic and container stations. Compared with cables, the system allows to distribute large amounts of electricity even in limited space and therefore connects the transformer and inverters securely and economically.
In addition, Fluence, a Siemens and AES company, will be on site to talk about its energy storage platforms and services, and how utilities, communities and industrial customers can benefit from scalable, flexible and cost-effective storage solutions.
Solutions for decentralized energy systems
Supply security, energy costs and a sustainable reduction in CO₂ are crucial to economic feasibility and competitive strength, especially in industrial applications, industrial parks, large buildings and municipal facilities. Siemens supports customers in all industries and sectors to implement efficient energy solutions: for example, through a targeted use of local renewable power generation, CHP plants, and energy storage. Services include planning, installing and operating decentralized energy systems and digital solutions and consulting services for smart energy management. This approach transforms energy costs, supply security and CO2 reduction into variables that can be calculated over the long term in any energy consumer's business plan. The free, data-based Energy Configurator, which can be seen live at "The smarter E", allows individual optimization potential to be calculated and an initial system layout to be generated that can be used to significantly lower energy costs and improve the environmental balance sheet.
Energizing electromobility ecosystem
Electromobility is a key building block for a sustainable and integrated climate, energy and mobility strategy. Siemens offers end-to-end solutions for charging infrastructure and components, charge management systems as well as complete end-to-end solutions and consulting services. The SiCharge CC AC22 charging station for electric vehicles in compliance with the IEC standard, for example, ensures rapid charging in public or semi-public environments like parking structures, garages and hotel and company parking lots. It can charge electric vehicles in about 45 minutes for a range of 100 km, depending on the battery charging system used in the car. The charging stations simultaneously provide 22 kilowatts (kW) at two charge points and can be operated intuitively with an integrated display.
Our next generation charging unit for residential buildings and commercial parkings will also be presented at "The smarter E fair". It extends our residential Junelight and professional SiCharge portfolio. This smart charger, has a power output of up to 22 kW, is equipped with Wi-Fi and Ethernet interfaces, among other features, and can be automatically updated wirelessly. The charging unit can be easily mounted on walls or piles and makes it possible to measure and visualize consumption. Combined with our Junelight Smart Battery it allows electric cars to be charged reliably and quickly within about 45 minutes (for 100 km) using self-generated solar power in garages and car ports, for example.
To drive for operational excellence of charging infrastructure, Siemens provides tailored service offerings from technical operation to complete managed service packages. This includes performance guarantees for company fleet, real-estate owners and infrastructure operators, for example.
Smart energy management in buildings
Buildings, infrastructure facilities and industrial enterprises occupy a key position when it comes to transforming energy systems. As prosumers, they simultaneously consume, produce and store energy, and need an electrical infrastructure with technology designed for this purpose. Siemens offers a seamless range of systems and products for safe and efficient low-voltage power distribution in decentralized energy environments. This includes communications-capable protection and switching devices from the Sentron portfolio for protecting electrical equipment; a power monitoring system with measuring devices; software, and direct connection to cloud-based IoT systems, such as MindSphere, for monitoring and analyzing energy consumption; as well as intelligent storage solutions.
More information on "The smarter E Europe" at www.siemens.com/press/smarter-e-2019
For this press release

@Siemens_Energy
Siemens Smart Infrastructure (SI) is shaping the market for intelligent, adaptive infrastructure for today and the future. It addresses the pressing challenges of urbanization and climate change by connecting energy systems, buildings and industries. SI provides customers with a comprehensive end-to-end portfolio from a single source – with products, systems, solutions and services from the point of power generation all the way to consumption. With an increasingly digitalized ecosystem, it helps customers thrive and communities progress while contributing toward protecting the planet. SI creates environments that care. Siemens Smart Infrastructure has its global headquarters in Zug, Switzerland, and has around 71,000 employees worldwide.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of power generation and distribution, intelligent infrastructure for buildings and distributed energy systems, and automation and digitalization in the process and manufacturing industries. Through the separately managed company Siemens Mobility, a leading supplier of smart mobility solutions for rail and road transport, Siemens is shaping the world market for passenger and freight services. Due to its majority stakes in the publicly listed companies Siemens Healthineers AG and Siemens Gamesa Renewable Energy, Siemens is also a world-leading supplier of medical technology and digital healthcare services as well as environmentally friendly solutions for onshore and offshore wind power generation. In fiscal 2018, which ended on September 30, 2018, Siemens generated revenue of €83.0 billion and net income of €6.1 billion. At the end of September 2018, the company had around 379,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Reference Number: PR2019050261SIEN
Contact
Heidi Fleißner
Siemens AG
Siemensstr. 10
93055 Regensburg
93055 Regensburg
+49 (941) 790-2212