Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Save time in engineering with the new Comos Version 10.3

Save time in engineering with the new Comos Version 10.3

Save time in engineering with the new Comos Version 10.3

The engineering portal in version 10.3 of Comos speeds up the engineering process. The portal can be reached directly in Comos from the product selector. The user quickly and easily enters all the requirements the component has to fulfill and selects the most appropriate option from the current product offers provided from a range of manufacturers. After downloading all the necessary information, the data sheets and specifications are imported into Comos from the engineering portal. For example, this allows the selected cable to be quickly and easily integrated into a circuit diagram – without any expensive and time-consuming customization. All information and documents are directly allocated to the component in Comos. This saves time during the engineering phase and bills of material can be generated fast. Potential sources of error are reduced as are any rectification costs. The Comos Engineering Portal is available in German, English, and Chinese.
Users can now modify the web application of the Comos software solution to suit their own individual requirements. Engineering data from Comos can now be easily integrated, edited, and validated and then being reimported into Comos. This provides greater flexibility and mobility in the design of workflows. For the first time, Comos Version 10.3 also allows object queries to be edited and batch processes to be completed in the Comos web application. The new 2D client makes it possible to call up objects in Comos without any previous revision. The data is therefore always up to date and can be seamlessly visualized in 1D, 2D or 3D. This provides the user with extremely high transparency and minimizes sources of error at the same time.
In addition to this, Comos makes it possible to consistently implement modularized engineering for all disciplines with central data storage and the use of intelligent templates – from tender preparation and engineering all the way to project completion. Using smart templates engineers and operators have access to a high degree of bidding and planning efficiency. Quotations can be compiled quickly, creating a solid base for a clear and structured cost calculation. Significant amounts of the basic engineering are already complete when the order arrives. So-called over-engineering or under-engineering can be substantially reduced by using the Comos modularized engineering solution. The standardized modules allow customer requests to be individually and concisely implemented. Regulatory requirements such as compliance can also be safely included. Comos allows companies to build up a solid knowledge base, secure their expertise, and remain successful for the long term.

For further information on Comos Version 10.3, please see www.siemens.com/comos10.3
For further information on Siemens at the Hannover Messe 2019, please see www.siemens.com/press/hm19 and www.siemens.com/hannovermesse
Siemens Digital Industries (DI) is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI's unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has around 75,000 employees internationally.
Read more
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of power generation and distribution, intelligent infrastructure for buildings and distributed energy systems, and automation and digitalization in the process and manufacturing industries. Through the separately managed company Siemens Mobility, a leading supplier of smart mobility solutions for rail and road transport, Siemens is shaping the world market for passenger and freight services. Due to its majority stakes in the publicly listed companies Siemens Healthineers AG and Siemens Gamesa Renewable Energy, Siemens is also a world-leading supplier of medical technology and digital healthcare services as well as environmentally friendly solutions for onshore and offshore wind power generation. In fiscal 2018, which ended on September 30, 2018, Siemens generated revenue of €83.0 billion and net income of €6.1 billion. At the end of September 2018, the company had around 379,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Read more
Reference Number: PR2019040189DIEN

Contact

Evelyne Kadel

Siemens AG

Klaus-Bungert-Str. 6
40468 Düsseldorf

+49 (211) 69161003