Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser
The world’s first SICHARGE FLEX charging system was officially put into operation at the OMV station in Kufstein on September 29, 2026.

The new SICHARGE FLEX system in Kufstein initially offers four charge points for passenger cars and two charge points for trucks, each with a capacity of up to 400 kW. In the next phase, four additional charge points for trucks will be added, with power outputs ranging from 600 kW to 1,200 kW delivered via MCS. This will significantly reduce the charging time. For example, a modern electric truck with a 620-kWh battery can be charged from 20 percent to 80 percent in about 45 minutes, allowing drivers to make the most of their legally mandated rest breaks. Thanks to fully dynamic power distribution, the available charging power can be allocated among the connected vehicles as needed.

Press Releases

Product Pictures

Press Pictures Opening

Peter Vysny (Vice President eMobility, OMV Downstream GmbH), Marcel Rümenanpf (Head of Sales EU Siemens eMobility), Michal Kubinec (Head of Retail Austria, OMV Downstream GmbH) Rene Zumbtobel (Landesrat Tirol), Gerrit Pürstl, Head of Siemens eMobility Austria, Matthias Medwenitsch, ( (Department Manager E-Mobility AT, OMV Downstream GmbH)

Parallel truck charging at OMV site in Kufstein

SICHARGE FLEX CCS Dispenser Column, Liquid Cooled

Video

Further Information

Contact

Christian Wilson

Siemens Smart Infrastructure

+49 172 1385608