Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release19 August 2015Siemens AG
Siemens lands €470 million order for substations in Qatar
“We are very proud that KAHRAMAA has chosen our field-proven and state-of-the-art products for Phase XII. We are working very closely to support the expansion of Qatar’s power distribution network with appropriate equipment and solutions,” said Wolfgang Braun, Senior Executive Vice President, Energy Management, Siemens Middle East. “These are highly challenging infrastructure projects in which a wide assortment from our portfolio of products and systems will be deployed. They are also highly demanding in terms of project management, because several systems will have to be constructed in parallel within a very short time.”
The order encompasses the design, engineering, supply, installation, and commissioning of 14 new substations for the 400-kilovolt (kV), 132-kV, 66-kV, and 11-kV voltage levels, including switchgear, transformers, control and protection equipment, and the extension of four existing substations.
The newly built 400-kV Bul Hemmaid substation will be used to transmit power from the independent water and power plant (IWPP) Facility-D into Qatar’s power grid. Facility-D, which will be fully operational by 2017, will have a power generation capacity of 2,400 megawatts (MW) and a desalination capacity of 130 million gallons a day (g/d) of water. Construction of the 400-kV Super Substation Al Sakhamah – which will feed power to various areas including Lusail Metro Primary in Lusail City – is also part of the contract. Lusail City will be hosting the inauguration and closing ceremonies of the FIFA World Cup 2022. All substations are required to supply power for ongoing infrastructure development projects, schools, hospitals, and residential complexes for the upcoming World Cup and Qatar’s National Vision 2030. The substations are located in and around Doha, the capital of Qatar.
Siemens’ new 420-kV single-break design 8DQ1 gas-insulated switchgear (GIS) will be used for the first time in Qatar. This system features a compact design and has a standard panel width of 2.20 meters, making it the smallest switchgear in the 380-kV (kilovolt) range. The 8DQ1 GIS systems will be manufactured in Siemens’ switchgear plant in Berlin, Germany. The transformers will be delivered from the transformer factory in Zagreb, Croatia.
Siemens will execute the order as part of the ongoing Qatar Power Transmission System Expansion – Phase XII. Since the beginning of the program in 2005, Siemens has installed more than 110 substations and approximately 1,400 kilometers of high-voltage cable. Siemens has completed all projects to date, totaling nearly €2 billion, within the defined schedule.
For this press release
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world’s largest producers of energy-efficient, resource-saving technologies, Siemens is No. 1 in offshore wind turbine construction, a leading supplier of combined cycle turbines for power generation, a major provider of power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2014, which ended on September 30, 2014, Siemens generated revenue from continuing operations of €71.9 billion and net income of €5.5 billion. At the end of September 2014, the company had around 343,000 employees worldwide on a continuing basis. Further information is available on the Internet at
www.siemens.com.