Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release19 April 2017Siemens AG
Siemens expands open cycle power plant in Kuwait with steam turbine
Picture: SST-800 steam turbine
An open SST-800 steam turbine at final assembly in Goerlitz, Germany. The SST-800 steam turbine and the SST-500 increase the capacity of the Az Zour South 3 plant in Kuwait by around 263 megawatts.
Siemens has received an order to deliver an industrial steam turbine package to expand the Az Zour South 3 open cycle gas turbine power plant to a combined cycle power plant. The plant is located in Kuwait and is operated by the Ministry of Electricity & Water (MEW). Siemens’ customer is the Chinese EPC contractor SEPCOIII. The expansion will increase the total installed capacity of the plant by 263 megawatts (MW) without using any additional gas. The combined cycle power plant is expected to go into operation in mid-2019.
Az Zour South 3 began operating as an open cycle power plant with two
SGT5-4000F gas turbines in 2015. Siemens is now supplying an SST-800 steam turbine (high pressure) combined with an SST-500 steam turbine (low pressure) and an SGen1200A generator for this stage. After the steam turbine expansion the hot waste gases of the gas turbines will be used to produce steam which will feed the turbo set. This will increase the plant’s total capacity by 263 MW without any additional gas consumption and will boost its efficiency significantly.
SGT5-4000F gas turbines in 2015. Siemens is now supplying an SST-800 steam turbine (high pressure) combined with an SST-500 steam turbine (low pressure) and an SGen1200A generator for this stage. After the steam turbine expansion the hot waste gases of the gas turbines will be used to produce steam which will feed the turbo set. This will increase the plant’s total capacity by 263 MW without any additional gas consumption and will boost its efficiency significantly.
“With our industrial steam turbine, we have developed a cost-effective and highly efficient solution for expanding the power plant,” said Jeffrey Dunlap, head of sales for the Middle East & North Africa region at Siemens Power and Gas. “With more than 263 MW, the additional capacity is outstanding for a non-reheat process. The project highlights the flexibility and individuality of these steam turbine expansions.
With our wide range of industrial and utility steam turbine portfolio, we will always find the right match to meet the individual steam tailing project targets.”
“Siemens has supported us strongly in winning this important contract and we are confident that this project will be a success story for SEPCOIII and all involved parties,” stated Wang Jianming, head of Procurement of SEPCOIII.
The customer SEPCOIII has already used Siemens’ steam turbine technology for three solar thermal power plants in Morocco. The Noor II project also operates with a combination of the SST-800 and SST-500.
Siemens components are already installed in the first and second stages of the Az Zour South power plant. The company supplied a total of eight SGT5-2000E gas turbines and two SST5-4000 steam turbines for this project.
This press release and a press picture are available at www.siemens.com/press/PR2017040266PGEN
For further information on the Power and Gas Division, please see www.siemens.com/about/power-gas
For further information on the Steam Turbines business unit, please see www.siemens.com/steamturbines
For this press release
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.