Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release25 October 2016Siemens AG
First Siemens Integrated Drive System (IDS) in the Middle East
The IDS, installed for the first time in the Middle East, is a unique technology from Siemens which allows the entire drive system in a manufacturing chain to be seamlessly integrated. The system will increase Qatar Steel's annual production by up to 3.7 percent.
Mr. Ali Bin Hassan Al-Muraikhi, Qatar Steel's Managing Director and General Manager said: "Boosting our output and reducing the maintenance and troubleshooting time are becoming increasingly important for us to improve our manufacturing operations. We are pleased to be the first company in the Middle East to implement this innovative Siemens technology, which is distinguished by its efficiency and reliability.”
“Through using an integrated drive system to streamline our rolling mills operations, we look forward to improving our performance and realizing the required efficiency, in terms of operations and productivity,” Mr. Al- Muraikhi added.
“This is a landmark installation for the Middle East’s manufacturing sector. An Integrated Drive System is capable of significantly transforming the productivity of manufacturing facilities, and we are proud that Qatar Steel is the first company in the Middle East to use this technology,” said Bernhard Niessing, Senior Executive Vice President, Process Industries and Drives, Siemens Middle East.
“As Qatar’s economy diversifies, the efficiency and reliability of its manufacturing sector is of increased importance. Innovative technology such as the Integrated Drive System is a key contribution to ensuring our customers in the region are getting the most out of their facilities, and operating at their most competitive.”
The productivity gains are mainly due to a marked reduction in maintenance shutdown time and complexity, as the IDS allows for flexible maintenance cycles. A reduction in troubleshooting time by up to 20 percent also means that potential problems are diagnosed faster, and major maintenance cycles can be better planned for. Moreover, the plant-wide standardization of Siemens machinery means that there is less downtime as parts are readily available. All these factors will lead to a faster time to market for Qatar Steel.
Siemens Integrated Drive Systems are the world‘s first true one-stop solution for entire drive trains. They enable noticeably shorter time to market and shorter time to profit. Integrating seamlessly in any drive train, any automation environment, and even in the entire lifecycle, Siemens IDS turn common drive components into drive systems and make assets become drivers of success. The result is less wear on machinery, easier diagnosis of potential errors and a more flexible approach to maintenance. Additionally, spare parts are available from a single source.
Formed in 1974 as the first integrated steel plant in the Arabian Gulf, Qatar Steel began commercial production in 1978 and it is now widely recognized as a leader in the steel industry locally and regionally.
For more information on Process Industries and Drives, please visit:
http://www.siemens.com/about/en/businesses/process-industries-and-drives.htm
http://www.siemens.com/about/en/businesses/process-industries-and-drives.htm
For this press release
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than200 countries, focusing on the areas of electrification, automation and digitalization. One of the world’s largest producers of energy-efficient, resource-saving technologies, Siemens is No. 1 in offshore wind turbine construction, a leading supplier of gas and steam turbines for power generation, a major provider of power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2015, which ended on September 30, 2015, Siemens generated revenue of €75.6 billion and net income of €7.4 billion. At the end of September 2015, the company had around 348,000 employees worldwide. Further information is available on the Internet at
www.siemens.com.