Steam turbine SST5-5000
Two SST5-5000 steam turbines to be installed in the new steam power plant at Attarat Um Ghudran, Jordan
Siemens will supply the key components for the Attarat steam power plant in Jordan. The customer China Energy Engineering Group Guangdong Power Engineering Co. Ltd. will build the facility as general contractor for the operator of the plant, the Attarat Power Company. Siemens’ scope of supply comprises two SST5-5000 steam turbines, two air-cooled SGen5-1200A generators, and the
turbine control system. The condenser is air cooled to address the lack of water at the site. This can be seen as a global trend for dry areas where water is mainly used for households, farming and ecosystem. The power plant will start operation in mid-2020 and will feed up to 470 megawatts to Jordan’s power grid.
The Attarat facility will supply enough electricity to cover up to 15 percent of the country’s annual power demand. Jordan is one of the most water-scarce countries in the world. The air cooled condensers will save up to 90 percent of the water needed for the plant’s operation compared with the use of a wet cooling system. Siemens will supply low-pressure turbines which are able to withstand the high back pressure caused by the condensers. The SST5-5000 is the most compact steam turbine generator consisting of one combined high- / intermediate pressure and one low pressure module ever built for a steam power plant. This will provide a small footprint and highest possible performance.
“The efficient use of water is a decisive challenge for this project, and with our modern technology we’ll provide the right equipment to achieve the highest electricity output and simultaneously save precious resources,” said Jean Claude Nasr, head of sales for the Middle East & North Africa Region at Siemens Power and Gas. “Along with our partner we will support the government’s plan to provide a reliable power supply and make Jordan less reliant on imported electricity.”
Jordan is considered one of the driest countries in the world, and 14 percent of the country’s power capacity is used for water treatment and distribution. The power plant will be built in the desert at Attarat Um Ghudran, 100 kilometers southeast of the Jordanian capital Amman and away from the country’s natural water supplies. The efficient use of scarce resources, especially water, is a critical challenge to provide a reliable power supply for the local population and economy.
“Siemens is the reliable partner to face the challenges of this demanding power plant project,” said Wenfeng Zhang, Deputy General Manager from China Energy Engineering Group Guangdong Power Engineering Co. Ltd. International. “They provide proven power plant technology and vast experience in project management. Together we will help increase Jordan’s power generation capacities and lay the foundation for the future development of the country.”
This press release and a press picture are available at
www.siemens.com/press/PR2017060317PGEN For further information on the Power and Gas Division, please see
For further information on the Steam Turbines Business Unit, please see
www.siemens.com/steamturbines