Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release16 December 2014Mumbai
Siemens Ltd. surpasses 100,000 milestone for energy-efficient industrial motors
Becomes the first company in India to achieve this distinction for IE motors. Energy savings through the use of these motors is 300GWh, which is equivalent to power required by 80,000 average Indian households in an entire year. In 2012, Siemens was the first company in India to launch a complete range of locally-manufactured IE2 and IE3 efficiency class energy efficient motors.
Mr. Dirk Hoke, CEO, Large Drives, Siemens AG presenting the 100000th Motor to Mr.K.C.Sharma, Vice President E & I Projects, UltraTech Cement Ltd.
Siemens Limited announced that it has surpassed a key milestone in manufacturing and delivering International Efficiency (IE) class industrial motors by handing the 100,000th motor to UltraTech Cement Ltd. in Mumbai. This translates to energy savings of 300GWh, which is equivalent to the power required by 80,000 average Indian households for an entire year, since the launch of the motors in January 2012.
Siemens Limited was the first company in India to launch locally-manufactured IE2 and IE3 efficiency class energy efficient industrial motors; IE3 is currently the highest efficiency class as recognized by Indian Standards. These motors are capable of offering energy savings of up to 10% depending on the frame sizes when used in place of standard efficiency (IE1) motors.
“Energy costs are steadily rising over the last few years and will continue to rise as consumption grows. This has compelled industrial units, especially those that rely heavily on processes, to invest in energy-efficient equipment like energy-efficient motors. The IE class energy efficient industrial motors from Siemens help customers improve their business performance, reduce lifecycle costs, and meet environmental regulations. The achievement of this milestone only reiterates the growing awareness and need for such motors by our customers,” says Bhaskar Mandal, Country Division Lead, Process Industries and Drives, Siemens India.
For this press release
Contact
Bijesh Kamath
Siemens Ltd., Media Relations
phone: +91 22 3967 7537, 3967 7000