Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release18 January 2012Mumbai
Siemens launches new range of Betagard Miniature Circuit Breakers (MCBs) and Distribution Boards (DBs)
Among the unique features of MCBs from Siemens is the patented Slide Latch Release (SLR) feature for removal of MCB from DIN rail without use of any tools. The range is unique, presenting a highly effective touch protection against accidental contact, enabling easy firm mounting of bus bar with its wires in front for easy accessibility. Products are designed and manufactured in India in Siemens Aurangabad - a state of art, highly automated factory. These newly introduced products are ROHS (restricted of hazardous substances) compliant.
Siemens Betagard DBs have various features and enhanced aesthetics which make it highly presentable, user-friendly, are easy to install and reduces downtime during maintenance. The range offers options such as Single Door, Double Door and Double Door with Acrylic Window. A range of accessories like Wire Way Boxes and PPI assembly set provides users the flexibility of converting the DBs to offer higher degree of protection and amend configurations at site with ease. In addition, the detachable DIN Rail assembly enables easy mounting of devices, neat wiring and comfort in modification.
DBs are type tested at 3rd Party Government and Neutral Testing laboratories for Ingress protection (IP), Mechanical Impact Index (IK), Short Circuit Withstand Capacity (CSC) and Resistance to corrosion as per IEC 61439 -1. Also series of tests are performed at internal laboratories for achieving conformance to IEC standards.
The MCB range from Siemens: Range: 0.5 to 63 A Characteristics: B and C Single Pole, Double Pole, Triple Pole, Four Pole
The DB range from Siemens: Metal Enclosures SPN Single Door IP 20 DBs SPN Metal Double IP 43 Door DBs SPN Acrylic Double Door IP 43 DBs SPN Single Door IP 20 DBs SPN Metal Double Door IP 43 DBs SPN Acrylic Double Door IP 43 DBs Wire Way Boxes for IP 20 and IP 43 DBs TPN to PPI Conversion assembly set
The Siemens Infrastructure & Cities Sector (Erlangen, Germany) with approximately 87,000 employees offers sustainable technologies for metropolitan areas and their infrastructures. Its offerings include integrated mobility solutions, building and security technology, power distribution, smart grid applications, and low- and medium-voltage products. The Sector comprises the Divisions Rail Systems, Mobility and Logistics, Low and Medium Voltage, Smart Grid, Building Technologies, and Osram AG. For more information, visit http://www.siemens.com/infrastructure-cities
About Siemens Ltd.:
Siemens Ltd., in which Siemens AG holds 75% of the capital, is the flagship listed company of Siemens AG in India. Siemens in India including Siemens Ltd. comprises 17 legal entities, is a leading powerhouse in electronics and electrical engineering with a business volume aggregating about Rs. 12,000 crore. It operates in the core business areas of Industry, Infrastructure & Cities, Energy and Healthcare. It has nation-wide sales and service network, 20 manufacturing plants and employs about 17,500 people.
For this press release
Contact
Dr. Armin Bruck, Managing Director
Siemens Ltd.
130, Pandurang Budhkar Marg,
Worli, Mumbai - 400 018.
India
Worli, Mumbai - 400 018.
India
Tel. : (022) 3967 7000
Fax : (022) 3967 7500
Mr. Viswakumar Menon
Corporate Communication - Press Office
130, Pandurang Budhkar Marg, Worli, Mumbai - 400 018.
India
India
Tel. : (022) 3967 7537 / 3967 7026
Fax : (022) 3967 7174