Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release08 March 2018Mumbai
Siemens installs state-of-the-art steam turbine for Shakambhari Ispat & Power Limited
Siemens Limited completed the supply, installation and commissioning of an 8.5 MW steam turbine, gear box and related control panels for Kolkata-based Shakambhari Ispat & Power Limited, one of the leading manufacturers of steel and supply of power. This installation is in addition to an 8 MW steam turbine that was delivered in a record time of three months.
"Being part of a steel producing plant, continuous operation has always been a concern for us. The association with Siemens has given us access to a wide variety of technically superior solutions which address our primary concern. The use of efficient turbines has already reduced consumption of coal. Moreover, solutions such as Remote Diagnostic System, Combustion Optimizer and new-age control systems will definitely reduce the downtime of the plant and turn it into a more profitable unit,” said Deepak Kumar Agarwal, Chairman and Managing Director, Shakambhari Ispat & Power Limited.
“Growing energy demand and rising energy prices make investment in turbines economically viable. The modular design concept of the installed steam turbines ensures high flexibility, availability and a reduction of time-to-market. Implementation of such cost-efficient solutions can lead to a gradual transformation of existing plants, helping manufacturers secure operational benefits over the long term, The state-of-the-art Siemens technology is also supporting in reducing the carbon footprint of our customers,” said Prashant Jain, Head, Power Generation Services, Siemens Limited.
The industrial power sector has witnessed a remarkable growth in the last couple of years. The demand for power and energy continues to rise and related energy costs have kept pace. The efficient utilization of available energy sources has become essential and many industrial companies are prospecting for opportunities and solutions for improving efficiency or reducing costs. Siemens Steam turbines can be instrumental in meeting targets of improved efficiency or reduced costs in industrial power plants.

For this press release
Contact
Bijesh Kamath
Siemens Ltd., Media Relations
phone: +91 22 3967 7537, 3967 7000